Other Parts Discussed in Thread: MSP430FE4232 Why The program stops execution after i terminate the debugger session MSP430FE4232 ?
I have a problem with the part number MSP430FE4232 everything works ok with the program and i debug it fine but the strange…
I was looking at the datasheet to see how to handle or adjust my voltage so that no negative voltage is applied to the inputs of the ESP430. But I noticed that there is nothing like that done. I it safe for me to apply AC to the analog inputs and exactly…
Other Parts Discussed in Thread: MSP430FE4232 hi I want to use the MSP430FE4232 for phase-phase energy metering. Is it possible? Can I set the register "phase correction", which adjusts the angle between voltage and current, to adjust metering for phase…
Other Parts Discussed in Thread: MSP430FE4232 Hi,
I would like to measure only RMS voltage (no current measurment required) using MSP430FE4232 with following conditions
a) 1 reading / sec is not acceptable to me when SD16OSR = 256 fM = 1.048576…
Other Parts Discussed in Thread: MSP430FE4232 Hi,
I would like to measure only 0 - 500 V AC RMS using MSP430FE4232 (SD16).
How do I configure SD16 and ESP430 ? Does RMS measurement and calculation happens in hardware ESP430, once configured …
Other Parts Discussed in Thread: MSP430FE4232 Question: I would like to use the MSP430FE4232 as a standard microcontroller with delta sigma. I don't want to use the signal processing capability of the ESP module which is tailored for e-metering applications…
Hi, Thanks for your feedback which was of immense use. There is one more issue pending :-
Thanks for code composer studio of higher version [ CCS 5.5.0.00077].
We have install the same & our observation are as follows with controller MSP430FE4232…
Other Parts Discussed in Thread: MSP430FE4232 hi
I'm trying to use the MSP430FE4232 for phase-phase energy metering. For this type of metering, it's necessary to delay the current at 90º. I use the equation of the page 21 from ESP430CE's datasheet for…
The MSP430FE4232 uses only the 4-wire JTAG interface and does not support the Spy-Bi-Wire interface.
To support the 4-wire JTAG, the MSP-FET430UIF tool needs to be used.
Aravind, The two microcontroller products that are included in the launchpad are these: * MSP430G2211IN14 – 2kB Flash, 128B RAM, 10 GPIO, 1x 16-bit timer, WDT, BOR, Comparator A+ * MSP430G2231IN14 – 2kB Flash, 128B RAM, 10 GPIO, 1x 16-bit timer, WDT,…