Part Number: MSP430FR2310 Other Parts Discussed in Thread: DRV10983 Hi team,
I'm writing motor parameters to the DRV10983 from the MSP430FR2310PW16R via I2C. If I keep writing to the EEPROM of the DRV10983, about once every few to several tens of times…
Part Number: MSP430FR2310 Other Parts Discussed in Thread: MSP430FR2311 , MSPM0C1103 , Tool/software: I have a design that is about 80% done on an MSP430FR2311 -- I use all of the peripherals on-chip to minimize design component count. I like the part…
Part Number: MSP430FR2310 When the VCC voltage is 2V, use pin P1.5 to output a high level to drive a MOSFET, and then enter the LMP4 state. When the VCC voltage drops by 1.5V, can P1.5 still maintain the output high level?
We understand that it is possible…
Part Number: MSP430FR2310
Hi,
In the MSP430FR231x datasheet (revision E), in table 6-22 on page 60, the input channels of the transimpedance amplifier are described to only use P1.7 (TIA0+) as positive input, all other input channel selections are…
Part Number: MSP430FR2310 Other Parts Discussed in Thread: ENERGYTRACE The complete IC model is msp430fr2310irgyr.We have an LED product using this model. In order to test the power consumption of lpm3, we deleted some circuit components, and finally…
Part Number: MSP430FR2310 Our customer has an LED product, which needs a key input, a PWM output, and an ADC. The msp430fr2310i was used before, and now there is a demand for 200kpcs. The low-cost scheme is required. The target is 0.13usd. Is there a…
Part Number: MSP430FR2310 I'm having an odd issue; my port 1 interrupts will not clear. From the moment I call _enable_interrupt() I execute no more code other than in an interrupt handler - if I place a breakpoint on the statement following this I never…
Part Number: MSP430FR2310 Team,
we are looking for a low cost MCU with 3 channel DAC, also ADC (3 ch or more) and an integrated op-amp (optional).
In some variants there is the Timer_B output that can be used as 1x DAC, then there is the integrated…
Part Number: MSP430FR2310 Hi experts,
Like the original question, my customer is trying to implement SPI-to-I2C bridge on MSP430FR23xx,FR2433.
Why is there no sample code for SPI-to-I2C bridge in " MSP430-FUNCTION-CODE-EXAMPLES "?
The UART-to-UART…
Part Number: MSP430FR2310 Customer is looking to implement a low power counter that can toggle an output after 12 hours of being powered up. Target current consumption is 300 nA.
The MSP430FR2310 looked like a good fit, but it consumes 0.71 uA in LPM3…