Part Number: MSP430FR2310
I am using the battery to power on msp430fr2310.battery was drained completely . I Have charged the battery to max voltage .at that state code in the msp430 is not working.if we given the power cycle to msp430 then only msp430…
Part Number: MSP430FR2310 We have a product that uses the timer function of MSP430FR2310, and the P1.6 pin uses the IO function to output high and low levels to generate a PWM signal. During our test, we found that we got 10KHZ, 10% signal when using…
Hello,
I haven’t heard back from you, I’m assuming you were able to resolve your issue. If not, please provide post a reply with an update below (or create a new thread).
thanks,
ki
Part Number: MSP430FR2310 Other Parts Discussed in Thread: MSP-FET , UNIFLASH Tool/software: TI C/C++ Compiler Hi
I write the MSP430 program to the CPU with CCS. Which file is created by compiling?
I would like to send a data file from our company…
Part Number: MSP430FR2310 From the user guide, I have noticed the register to be 8 bit.
My doubts are :
Does setting each bit represent the interrupt action in the corresponding pin of the port ?
If so, can only one bit be SET in the PxIFG register…
Part Number: MSP430FR2310 Hello,
Can you confirm that we can run up to a 1kHz pulse stream from one of the GPIO pins to Timer_B3 in LPM3 (Standby power mode, Low Power Mode 3) for the MSP430FR2310? It seems from the datasheet that if this is possible…
Part Number: MSP430FR2310 Hi
After program MSP430FR2310 by Xeltek programmer tool. Can't read out chip ID.
If remove below code, then programming and verification becomes successfully, but the chip don't work correctly.
Part Number: MSP430FR2310 Other Parts Discussed in Thread: BQ27541 TI Taiwan had indicated there is HQD code for the MSP430.
However, when the software team checked the HDQ sample code, it found the Timer needs the SCCI bit.
Only Timer_A can support…
Hi Victor,
Yes, the input impedance ought to be in the 100's of MΩ range based on the input bias being in the single digit nA range. The MSP430FR2310 in the TSSOP16 package actually has a dedicated inverting input on the TIA to provide a very low bias…