Part Number: MSP430FR2311 I have a problem while using MSP430FR2311 in IAR:
After creating a workspace and a new project, I tried to select target device in “Project” -> “Option” -> “General Options” -> “Target” -> “Device”. While in Texasinstrument category…
Part Number: MSP430FR2311 Hi,
I am using MSP430FR2311 for my project.I want to use RTC in calendar mode.I am using driver library examples.Can you suggest how to set rtc in caledar mode because I didn't find any APIs for RTC in calendar mode in driver…
Part Number: MSP430FR2311 Other Parts Discussed in Thread: MSP-GANG I mass-produced a batch of products, using MSP430FR2311IPW16R. Use MSP-GANG to burn, burn 8 pieces each time, Unfortunately, many program failed.
So, I made the simplest circuit board, which…
Part Number: MSP430FR2311 Other Parts Discussed in Thread: MSP430FR6989 , MSP-EXP430FR2311 I was trying to use the CTPL with the MPSFR2311, but even with maximum optimization they do not seem to fit in the part. I can proceed without the library, but it…
Part Number: MSP430FR2311 Hello, I'm trying to set up my MSP430 to use an external 4MHz oscillator but it seems to be causing a fault, since the flag XT10FFG is set high on CSCTL7. Here is my set up code, can someone let me know what I'm doing wrong?…
Part Number: MSP430FR2311 Hello,
We are using the following code for transmitting data from UART. For this, we are using the MSP430FR2311 controller. After running our code, we are not receiving data on the serial monitor.
Thank You!
#include <msp430…
Part Number: MSP430FR2311 Hello,
I require information or a statement from TI regarding the use of "Voltage enhancement circuits" within the MSP430FR231x. In order to obtain certification for IECEx i need documented evidence that the MCU either…
Part Number: MSP430FR2311 Other Parts Discussed in Thread: MSP430FR2433 Hello, I am currently working on a system which can measure the variable frequency (100Hz - 2MHz) of a square signal. The MCU I use for my system is a MSP430FR2311. I found on dev…
Part Number: MSP430FR2311 Other Parts Discussed in Thread: MSP-EXP430FR2311 I have the MSP-EXP430FR2311 launchpad and as far as I can tell, DriverLib is supported, but the only examples I can see are for the MSP430FR4XXX.
Can someone point me to the correct…
Part Number: MSP430FR2311
Hi Team,
I'm compiling a project written in CCS version 11.1.0.00011 (written in asm) and the generated .hex assembly file on top contains the RAM data section (from addr 0x2000).
As I'm using that file for loading the code…