Part Number: MSP430FR2353 Since I am beginner to the MSP430FR2355 and want to send ADC data of MSP430FR2355 to the RealTerm in PC.Could u suggest me what kind of hardware connection and codes are required to send data from MSP430FR2355 to RealTerm with…
Hi Amit,
I understand, that from your point of view all this belongs to one project of yours, but this is not related to one and the same specific problem, but moving from one to another. Our strategy is to deal with each specific problem separately…
Part Number: MSP430FR2353 Other Parts Discussed in Thread: MSP-EXP430FR2355 , MSP430FR5994
Dear *,
we wan to use MSP430FR2353 for our project and have couple of questions regrading ADC and DAC
1) DAC
Can we use SAC0 OA in voltage follower…
Part Number: MSP430FR2353 Other Parts Discussed in Thread: MSPMATHLIB ,
Dear *,
is the MSP430FR2353 or MSPFR2355 supported in Floating Point Math Library for MSP430 ?
Because the description says:
MSP430 devices supported by MSPMATHLIB:
FRAM…
Part Number: MSP430FR2353
Dear *,
we have connected 24MHz oscillator on XIN pin of MSP430FR2353.
i'm unable to set the MCLK to 24MHz, i'm observing pin P2.6 as MCLK out and i'm getting 1MHz ( probably the fall-back mode)
Am i doing something…
Part Number: MSP430FR2353 Dear *,
our first MSP430 has a 24MHz oscillator (ECS-2520MV-240-BN) on XIN pin , and we want to output 24MHz on MCLK pin and connect it to second MSP on XIN pin, and so on 9 times .
Do you see any problem with this kind…
Part Number: MSP430FR2353 Hi Team
The customer would like to know that FLL lock time (Max) when DCO = 16Mhz with Internal REFO as reference?
Would you please provide it?
If you have not it, do you have a rough indication data or an approximate…
Part Number: MSP430FR2353 Dear *,
can you tell:
1) Do we need pull-up resistors on UART TX AND RX, and what value is recommended ?
2) Our MSP430 will be SPI Slave do we need Pull-up or Pull-down on any of SPI signals , and what valuse are recommended…
Part Number: MSP430FR2353 Hi Team,
The customer couldn’t write the program to FRAM after they program the device.
They could debug by CCS and write 0xA500 ( DFWP = 0, PFWP = 0) into SYSCFG0. But they are still not able to write into FRAM.
Is…