Part Number: MSP430FR2433 Other Parts Discussed in Thread: MSP-EXP430FR2433
Hi Team,
Posting on behalf of our customer.
I have this MSP-EXP430FR2433 and CCS installed. I have some code here, which Google Gemini helped me with. My goal is to run…
Part Number: MSP430FR2433 We have multiple TI-Gang programmers in use, running on 32-bit systems.
But now we are switching over to 64-bit systems (LabView) and are in lack of a 64-bit driver.
Maybe we are not looking in the right location but so far…
Part Number: MSP430FR2433 Other Parts Discussed in Thread: MSP-FET
Tool/software:
How do I program the MSP430FR2433 LaunchPad using the MSP-FET?
I would prefer to use the 2-wire JTAG.
What connections do I need to make between the MSP-FET…
Part Number: MSP430FR2433 Hello TI team,
We are doing a simple mutual-capacitance experiment (copper foil electrodes on acrylic plates, sandwiching a soft tube) to evaluate detection sensitivity before designing a dedicated electrode PCB. During a radiated…
Part Number: MSP430FR2433 Tool/software: Hi,
I would need to know, about max. temp. vs humidity ratings for the MSP430FR2433.
E.g. which max. temp. is allowed, with 95% rel. humidity?
I can't find a datasheet, where this would be specified.
…
Part Number: MSP430FR2433 Tool/software: I am trying to connect the launchpad to a new windows PC I just got. It only has USB3.2 and USB4 The launchpad connects fine on my old pc on USB2 I tried uninstall the CCS installation and re-install without change…
Part Number: MSP430FR2433 Other Parts Discussed in Thread: UNIFLASH
Tool / Software: CCS Category: MCU Subcategory: UART BSL Entry Issue
Description:
When attempting to invoke the BSL via the standard TEST/RST sequence , the MSP430FR2433 does not…
Part Number: MSP430FR2433 I'm working with MSP430FR2433 microcontroller and I want to implement ADC & PWM Output. Is there any examples code available for ADC & PWM Out module to get started? If Yes, please share.
Part Number: MSP430FR2433
Tool/software:
Hello,
May I have question about MSP430FR24xx register?
I think there is SYSRSTIV register for read cause of before time of reset.
Q1 :
Is there another register that can know before-reset cause?
…
Part Number: MSP430FR2433 Tool/software: Hello,
My customer is using MSP430FR2433xx.
I believe there is delay time between my setting PMMCTL2.INTREFEN and MCU set REFGENRDY.
Do you have max and typ [ms or µs] of specifications?
Thanks,
GR