Part Number: MSP430FR2533 Other Parts Discussed in Thread: MSP430FR2355 Recent design using MSP430FR2355 experiencing premature BOR threshold that forces loss of all programmed outputs at HIGH or LOW and then restart recovery that takes 168ms as measured…
Part Number: MSP430FR2533 Other Parts Discussed in Thread: MSP430FR2311 Hi Team
One of my applications involves getting pulse inputs from a hall sensor and sending a coded piece of information of this pulse on i2c or equivalent high speed serial interface…
Hello Eddie,
Tracing the proximity behaviour with Captivate connected via Uart to the MSP we found that the Conversation Count Value when touched goes below Proximity Threshold but Proximity in the in the above described Error case, is not detected …
Part Number: MSP430FR2533 Hi,
The MSP430FR2533 i2c slave stops responding to the master (QCC5124). We have an extremely high return rate of units experiencing this problem at 6%.
Some background on how we're using the MSP:
We are periodically sending…
Part Number: MSP430FR2533 Hi team
Could you kindly advise where is start address after MCU reset ?
The start address is fixed or not ?
Thank you and best regards,
Michiaki
Part Number: MSP430FR2533 Hello,
I'm reading BOR section in page of 26 in Datasheet.
But I can't understand about BOR operation.
Is my following understanding correct?
Only If DVCC drops below (VBOR, safe), and kept low longer than (tBOR, safe…
Part Number: MSP430FR2533 Hello,
I understand BSL of MSP430FR2533 supports only I2C and UART.
Are there any solution to update the firmware of MSP430FR2533 with SPI?
Regards,
U-SK
Part Number: MSP430FR2533 Hello,
Is there any limit to the fluctuation of power supply voltage so that CapTIvate can be touched functionally?
(ex. 3.3V ± ?%)
Regards,
U-SK
Part Number: MSP430FR2533 Hello,
The dimension between MSP430FR2533 and DC-DC converter is only 100mm.
Is it possible to cause any trouble to touch sensing of MSP430FR2533 due to the switching frequency of DC-DC converter (ex. RF noise)?
Regards,
U-S…
Part Number: MSP430FR2533 Hi,
We are using MSP430FR2533. In our design, we are using P1.4 as JTAG interface TCK, P1.5 as JTAG TMS, P1.6 as JTAG TDI and p1.7 as JTAG TDO. We are using remaining 4 bins (p1.0 – p1.3) as general output. During the initialization…