Part Number: MSP430FR4131 Tool/software: Hello TI technical Support Team,
I recently made a purchase through the Web, but I noticed that the order was marked as "cancelled" on TI store platform. When I reached out to the customer support, I was informed…
Part Number: MSP430FR4131 Tool/software: Hello.
I am using CCS V12.6.0.00008 & msp430fr4131. I have a weird FRAM usage in this code:
// Built with Code Composer Studio v12
//*******************************************************************…
Part Number: MSP430FR4131 Hi team,
Do we have sample codes which control LCD driver in MSP430FR4131? My customer would like to use sample codes without any modifications.
Best regards,
Shunsuke Yamamoto
Part Number: MSP430FR4131 Hi team,
Do we have sample codes which control LCD driver in MSP430FR4131? My customer would like to use sample codes without any modifications.
Best regards,
Shunsuke Yamamoto
Part Number: MSP430FR4131 The application manual states the formula for the ADC conversion as :
N=1024 (Vin-Vr-)/(Vr+ - Vr-)
Is there a minimum value for the Vr+ - Vr- difference that is required for a reliable ADC operation. E.g. will the ADC produce…
Part Number: MSP430FR4131 In order to mitigate cs13 with workaround 4, is it enough to set the DCO to 2 MHz or does it actually have to run at 2 MHz? Assuming, we are running at 16 MHz (DCORSEL = 101b), the following code
bis #LPM3_bits, 0(SP)
bis #SCG0…
Part Number: MSP430FR4131 Hi everyone,
I have connected an LCD to MSP430 microcontroller. I am using LCD_E controller and external charge pump capacitors (0.1 uF). I have configured everything correctly.
I have 4 COM pins, when I turn off a segment…
Hi Teach Me,
Although true that the MSP430FR4131's LCD peripheral only supports segmented LCDs, the TFT2N0369-E module includes a driver IC (SSD1289) that supports SPI and parallel interfaces. Therefore almost any MSP430 is compatible with this LCD…
Hi,
Based on those peripherals, I would suggest that you look at the MSP430FR4133 (or MSP430FR4131 or MSP430FR41312 depending on how much memory you need). I do not believe you will find a device that is completely pin compatible, so you will probably…
MSP-GANG supports FR4133 from revision v1.1.10.0 which was released in Oct.2014.
If you go to the home page for MSP-GANG: www.ti.com/msp-gang , and click on button of "Get Software", you will come to the download page and it will show a description…