Part Number: MSP430FR4133 Other Parts Discussed in Thread: DRV5055 I am attempting to use the ADC on the MSP430FR4133 to display read results from the DRV5055 Linear hall effect sensor. I am running into an issue I think with initialization of the ADC…
Part Number: MSP430FR4133 Hello everyone. I'm trying to process some data using the MSP430FR4133 EVM, and i'm getting this issue where my variables are being written to the same register. This snippet of code i'm taking in some dummy array of 8 bit values…
HI Kieran,
It's been a few days since I have heard from you so I’m assuming your question has been answered. I will mark this posting as RESOLVED. If this isn’t the case, please click the "This did NOT resolve my issue" button and reply to this…
Part Number: MSP430FR4133 I'm currently working with the MSP430FR4133 launchpad. I found some code from the out of the box demo that set up timer a to be a debounce timer for the pushbuttons on the device. I attempted to use this for my project, and was…
Part Number: MSP430FR4133
I am executing a simple state machine that steps based on a pin change and sleeps between steps. A significant amount of time is spent in the overhead overhead of calling the ISR on each pin change, which increases latency and…
Part Number: MSP430FR4133
Hello.
I am testing a MSP430FR4133 chip with SPI. Clock freqs MCLK and SMCLK is 8MHz and ACLK is 32.768 KHz (all tested)
SPI init code is below;
GPIO_setAsPeripheralModuleFunctionInputPin(
GPIO_PORT_P1,
GPIO_PIN0 + GPIO_PIN1…
Part Number: MSP430FR4133 Other Parts Discussed in Thread: MSP430FR2033 What is the difference between the MSP430FR4133 and the MSP430FR2033?
Regards,
Loay Suffer
Part Number: MSP430FR4133
Hello
I use the msp430fr4133 mcu.
two seieal communication I used.(UART, I2C)
The I2C communication uses the msp430 as the master, and is being tested to read the register value through i2c every 10 seconds.
The problem is…
Part Number: MSP430FR4133 Everything is in the title, i use an MSP430 in a design where i routed the SBW interface to the main MCU, in the perspective of remote firmware upgrade.
I would like to implement this now and i wonder if there is some existing…
I read the Slaa654a.pdf, but my doubt can I control I 20x8 LCD using MSP430FR4133? Because it is not working with LCD. Today I am using Lcd Driver HT 1622 - 64LQFP and it is working.
Regards