Hi David,
You can find examples in our TI Resource explorer. Once you have selected your device you can choose 'register', where you directly program the specific register (bare metal), or you can choose the driver library, which uses an API (pre-written…
Part Number: MSP430FR5857 Other Parts Discussed in Thread: MSP-EXP430FR5994 Dear Sir/Madam,
I am using MSP430FR5857 micro-controller in my application . I am giving signal to coil of power relay (230V AC) to turn ON and OFF from microcontroller as per…
Part Number: MSP430FR5857 Dear Sir/Madam,
i am using microcontroller msp430fr5857 for the application EVSE. while using internal DCO clock for 16 MHz ,MCU working fine with no issue even with line and neutral interchange on power side but when we use…
Part Number: MSP430FR5857 Other Parts Discussed in Thread: MSP430WARE Tool/software: Code Composer Studio Dear Sir/ Madam
I have configured external crystal to the HFXTIN pin and HFXOUT of 16 MHz ,18 pf,external capacitor values connected are 30pF i…
Hey Priyanshu,
Have you seen our ADC code examples in CCS? You can find these by navigating to:
View > Resource Explorer > Software > MSP430Ware > Devices > MSP430FR5XX_6XX > MSP430FR5857 > Peripheral Examples > Register Level
There you will find…
Part Number: MSP430FR5857 Hello sir,
The query is related to MSP430FR5857 microcontroller which is used to give signal to turn ON and OFF operation of MOSFET's connected in the relay 12V coil of 230V AC MAINS line and neutral relays.
Query:
…
Part Number: MSP430FR5857 Tool/software: Code Composer Studio Hello Sir
I am using MSP430FR5857 MCU . I am Using Texas Driver Library . I have tried to generate interrupt using timer TA1 using CCR1 but its not generating properly mean to say its generating…
Part Number: MSP430FR5857
Tool/software: Code Composer Studio
Dear Sir / Madam ,
I am using MSP430FR5857 MICRO CONTROLLER for my application. I am sensing AC voltage sensing, AC current sensing and PWM signal which is generated by microcontroller…
Part Number: MSP430FR5857 The PxSEL0 and PxSEL1 and used to select the function that the GPIO will work as. As only two bits are available only a max of 4 choices can be used.
But as you can see in a few pins there are a more than 4 functions for…