Part Number: MSP430FR5887 How to enhance the detection distance of ESI module to metal? What aspects should we start from?Which parameters to modify in the code
Part Number: MSP430FR5887 Tool/software: Code Composer Studio We used the following reset circuit for MSP430FR5887.
In the production line, we found that 1 of 100 board could not be pulled high. The final voltage is 1.7V~1.8V.
May you give me some suggestion…
Tool/software: Code Composer Studio //User need to switch on the motor with half-covered matal disc to finish the calibration Set_DAC(); Is there any requirement for the speed of the dial to calibrate the DAC when the dial rotates? If so, what is the speed…
Part Number: MSP430FR5887 Tool/software: Code Composer Studio Many manufacturers without magnetic sensor in the factory on the inductance surface affixed metal film, and some manufacturers did not stick.Does this metal membrane do anything?
Part Number: MSP430FR5887 Dear all:
I used MSP430FR5887 to design the magnet-free sensor. When my program was just written, I ran sample OK.But then the power went off and the sampling went haywire.
The power supply is 3V, I use the voltage regulator…
Hi Eduardo,
You are correct, the minimum pin count for devices the with ESI module is 64.
The following devices are also 64 pin devices with ESI module and no LCD module
MSP430FR5887
MSP430FR5888
MSP430FR5889
MSP430FR58891
MSP430FR5986
…
There are signs that the following members are coming. Any hint when?
MSP430FR4131, MSP430FR4132, MSP430FR4133 MSP430FR5887, MSP430FR58871, MSP430FR5888, MSP430FR58881, MSP430FR5889, MSP430FR58891 MSP430FR5986, MSP430FR5987, MSP430FR59871, MSP430FR5988…