Part Number: MSP430FR5969-SP Other Parts Discussed in Thread: MSP430FR5969 I am looking for Flight heritage for this part. Can you provide that please. Thank you
Part Number: MSP430FR5969 I am designing a board with three MSP430FR5969 all in seperate power domains on it that I am trying to program. Obviously I will have to buffer signals across the power domains. I have JTAG signals run to the board via LVDS differential…
TI might not even know. Given some of these programs, the final user might use a "blind-buy" system to obfuscate the actual end use. I know my company does that. (Though I have no knowledge as to whether any TI MCU's are involved).
Part Number: MSP430FR5969 Hello,
How much risk is there related to setting the optimization level to the max for my C++ project? Is it worth it to go with opt-level 4 or is leaving it at 3 or 2 enough. I wrote a Gpio library using constexpr and inlining…
Part Number: MSP430FR5969 Hello,
I am designing a custom circuit that uses the MSP430FR5969 microcontroller. For programming and debugging via JTAG , I would like to integrate an FTDI device on my board.
I am currently considering using the FT4232H…
Part Number: MSP430FR5969 Hi Experts,
Wanted some quick clarification on how the print speed based on 'counter' incrementation is calculated using the MSP430 Timer in the following code snippets:
In the main.c file:
In the sys_init.c file:
…
Part Number: MSP430FR5969 I am working on a program that requires reading the internal temperature sensor of the MSP430. Development was done on the MSP430FR5969 Launchpad, and now on a custom-built dev board, but I'm having issues reading the temperature…
Part Number: MSP430FR5969 Hello. I am working on sensor firmware where the state for the sensor logic is encapsulated in a C++ "Sensor" class. I would like the state of the class to be persistent across power cycles but initialized on program load. I…
Part Number: MSP430FR5969-SP HI,
I am looking for Space grade controller in MSP430 family with more then 64 IOs. Kindly suggest controller part number.