Part Number: MSP430FR59941 Other Parts Discussed in Thread: MSP430FR5994 Hi Team,
Our customer would like to confirm if it is possible to use the RTC of MSP430FR5994 without using an external crystal. I understand that the clock source for the RTC could come…
Part Number: MSP430FR59941 Does the MSP430FR59941 BSL (boot-strap) support a user configuration?
(I would like to use a different I2C address.)
Thank you
Part Number: MSP430FR59941 Other Parts Discussed in Thread: MSP-FET , I'm trying to reprogram an MSP430FR59941 using the BSL over the I2C bus. I am not using any password protection. I can program the same file into the chip with the MSP-FET tool.
…
Part Number: MSP430FR59941 The MSP is set up as a multi-controller. Another controller initiates a transfer and the MSP transitions to a peripheral. The transfer begins and a variable number of bytes into the transfer the MSP gets into a state where it…
Part Number: MSP430FR59941 We have a custom platform that utilizes an MSP430 chip that interfaces with another controller via I2C. After a period of high activity between the MSP430 and the controller, we have a situation where SCL is stuck low. When…
Part Number: MSP430FR59941 Hi,
i am trying to debug my program but im getting this error.
MSP430: Trouble Writing Memory Block at 0x1000 on Page 0 of Length 0x354: Could not write device memory
MSP430: File Loader: Verification failed: Target failed…
Hi Evan,
We are waiting for a fw modification to keep TEST low and to send the described waveform. As soon as we can confirm that it works we should be good to close this issue. Thanks for your help! I will update ASAP.
-Tony
Part Number: MSP430FR59941 I'd like to implement JTAG terminal. I have printf() messages in CCS CIO console but calling getchar() always return -1.
Can CIO console return input from user back to MCU or it is for STD output only?
Part Number: MSP430FR59941
What is the first value in the system reset register (screenshot from datasheet is provided below for reference) for MSP430 mean? When is this value expected?
How is value 00h and 02h (BOR) different. When I reset my board…
Part Number: MSP430FR59941 Other Parts Discussed in Thread: MSP430FR5962 , MSP430FR5964 , MSP430FR5994 , MSP430FR5992 , I am looking at this doc:
MSP430FR5994, MSP430FR59941, MSP430FR5992, MSP430FR5964, MSP430FR5962 SLASE54D – MARCH 2016 – REVISED JANUARY …