Part Number: MSP430FR6989 Hello,
I am currently testing the power consumption of the MSP430FR6989 when driving displays. In doing so, I want to compare an external voltage divider with the internal voltage divider to provide the bias voltage. However…
Part Number: MSP430FR6989 Hi,
I am trying to find a way to achieve firmware update handled by the firmware itself (without entering bootloader state). My idea is that I can have a function in my firmware that handles the firmware validation and writing…
Part Number: MSP430FR6989 Hi,
I recently bought a SX1262MB2CAS Lora module, I try to interface that module with MSP430.
I need to examples code for transmit and receive function.
kindly support us.
Thanking You........!
Part Number: MSP430FR6989 I have c++ code for MSP430 and ethernet configuration.
I included all the required files and file path to the project.
I can build the project without any error. While uploading the project to the controller I'm receiving error…
Part Number: MSP430FR6989 Other Parts Discussed in Thread: ADS1298 Dear All,
Good morning, I am working on a new product in which I have the MS430FR6989 microcontroller as the center of the design, with two external 32768hx crystals in LX and one 16Mhz…
Part Number: MSP430FR6989 I am using above mentioned microcontroller as Master SPI. Slave microcontroller receives command data from Master and sends its response. But Master could not receives the response data. And I'm using the standard master and…
Part Number: BOOSTXL-SENSORS
I have the MSP430FR6989 MCU and BOOSTXL-BASSENSORS connected. I believe the booster pack just needs to be on top of the MSP430 Launchpad as they are both 40 pin compatible. Assuming I have these connected correctly, I tried…
Part Number: MSP430FR6989 What setting should be made in the declarations of GCC version 12, or compiler options, so that during the build process it is checked that variables are defined with the same type in all the projec. files? example: in main.c …
Part Number: MSP430FR6989 Hey Guys,
I would like to know what kind of tool CCS is using to upload the C-Program, Assembler-Program or whatever to the MSP430FR6989. I know about the "mspdebug" and the "MSP430Flasher". Do you know which tool CCS is using…
Part Number: MSP430FR6989 Other Parts Discussed in Thread: EVM430-FR6989 , , MSP430WARE , MSP-EXP430FR6989 Hello ,
I recently purchased an EVM430-FR6989 Evaluation Module and I am interested in the default code that was pre-installed on the MSP430FR6989…