Part Number: MSP430FR69891
Tool/software:
Hi,
the memory information for the MSP430FR69891 is given at some places with 2k RAM and some other wit 8k.
Can you please clarify which info is right.
Thanks,
Stefan
Part Number: MSP430FR69891
We found that when URAT port short circuit, the program in the microcontroller will be erased, is there any way to avoid the program being erased
Part Number: MSP430FR69891 Other Parts Discussed in Thread: MSP430FR5989 , MSP430FR5969 Tool/software: Code Composer Studio I have a circuit with MSP430FR5989 and need to activate 3 SPI module UCBA1, UCB0, UCB1. Started to test UCB0 and UCB1 with pins as…
Part Number: MSP430FR69891 I am designing a circuit where I like to receive the firmware update using Bluetooth, store in the I2C memory for verification afterwards update the firmware(BSL) using I2C memory.
Is it possible with MSP430FR69891.
Help is…
Part Number: MSP430FR69891 Other Parts Discussed in Thread: MSP430FR6989 Hello,
I'm having difficulty placing variables in FRAM. I'm using the documented technique using the #pragma PERSISTENT feature of the compiler. When I do this, the variable…
Part Number: MSP430FR69891 Hello, I'm experiencing a problem with the design I'm working on which feels like an alignment problem. Basically, it looks like a global 16-bit value, which is in a structure isn't being written to or read from properly…
Part Number: MSP430FR69891 Tool/software: TI C/C++ Compiler Hello,
I'm experiencing a problem with the design I'm working on which feels like an alignment problem.
Basically, it looks like a global 16-bit value, which is in a structure isn't being…
Part Number: MSP430FR69891 Other Parts Discussed in Thread: MSP430FR6989
Hello
I am using the LaunchPad Eval Kit with the MSP430FR69891 uP.
I want to use the SPI Interface USCIA0 in slave mode, 4 pin mode active high, with clock phase flag UCCKPH=1…
First please check if you use msp430fr6989 or msp430fr69891 and they have different BSL interface as below
And if you have logic analyzer like Saleae, you can capture the signals on the communication bus and put it here.
Other Parts Discussed in Thread: MSP430FR69891 We’re reading through the MSP430FR69891 spec and wasn’t clear on how to program the inputs for the device. It indicates that there are internal pull-ups for the input lines but doesn’t indicate…