Part Number: MSP430G2101
Hi,
I couldn’t able to download and debug the MSP430G2101 micro controller USING IAR MSP430 with
FET debugger
Will you please support us to resolve this issue
We are using MSP430 IAR the below version
…
Part Number: MSP430G2101 I'm attempting to implement the following circuit. It's powered by 9v, which is passed through a momentary switch, and a voltage divider to bring the voltage down to ~2.7 volts. This voltage is used to enable a voltage regulator…
Part Number: MSP430G2101 Hi
We have an issue in our push-button application where we use the MSP430G2101IPW14. Communication is done over SPI which is very time critical. We have found out that in some push-buttons there is an SPI communication timing…
Part Number: MSP430G2101 Hello
My customer is using MSP430G2101/2201 in their products.
And now they are looking for the software's encryption algorithm.
could you help to provide the technical support on it ?
Thanks a lot
Other Parts Discussed in Thread: MSP430G2101 , UNIFLASH Hi three,
I am trying to program MSP430G2101 using UniFlash:
However, it fails to bring GUI and stuck on this window:
Any suggestions?
Thanks.
Stan
Other Parts Discussed in Thread: MSP430G2101 what kind of decoupling capacitor should be used for Msp430g2101. Please send me complete specification of it
Other Parts Discussed in Thread: MSP430G2101 I am trying to use a spy-bi-wire connection to program a MSP430G2101 from another processor. I have followed the manual (slau320g.pdf) and example code, but I cannot get any output from the MSP430. Right now…
Part Number: BQ500410A Other Parts Discussed in Thread: MSP430G2101 , , INA199 , TPS28225 , BQ51013B , BQ51050B Tool/software: Hello TI, I designed a board with a single coil and no MSP430G2101 Low Power Supervisor. I used the application diagram for…
Part Number: MSP430G2102 Other Parts Discussed in Thread: MSP430G2101 , CCSTUDIO , MSP-FET hello,
I'm trying to connect a "BlackHawk XDS560v2-USB System Trace Emulator" to an MSP430G2101.
I want to use LoadTI, but I get "SEVERE: MSP430: Error initializing…
Other Parts Discussed in Thread: MSP430G2101 CCS v5.5
MSP430G2101
MSP-FET430UIF
Hi there,
I have a custom board with G2101 which works fine with emulator connected even without simulation. It is just enough to have emulator connected. However…