Other Parts Discussed in Thread: MSP430G2101 Hello
I want to save two variables in segment B in flash of msp430g2101 .
When in saved variable x1 at address 0x1080 with following funcation call, it get saved.
But when i saved variable x2 at address 0x1084…
Other Parts Discussed in Thread: MSP430G2101 , MSP430F2101 I'm bringing up a board which uses the MSP430G2101 microcontroller, and I'm using IAR Kickstart. However, I don't see the device listed; the closest I see is the MSP430F2101. Is this…
Other Parts Discussed in Thread: TMS320F28335 , TMS320F2812 , TMS570LS3137 , CCSTUDIO , MSP430WARE , SYSBIOS , MSP430G2101 , MSP430G2230 , SHA-256 Hello,
I've got a problem with CCSv5.2 and 5.3. It randomly kills X window session. I'm using Debian testing with…
Other Parts Discussed in Thread: MSP430G2101 Dear Sir,
i am working on msp430g2101 with iar workbench ,i need to enable globle interrupt enable bit in status reg but here no SR is defined and this command is not working SR=(1<<3); or SR|=GIE ; showing…
Other Parts Discussed in Thread: MSP430F2101 , MSP430G2452 , MSP430G2101 Hi:
I´m using a Gang programmer to program MSP430Fxx with firmwaqre version 1.53, We need to program MSP430G2452 and MSP430G2101, I´ve made a upgrade of firmware to 1.54 firmware,…
Other Parts Discussed in Thread: MSP430F135 , MSP430G2101 , MSP430F5308
When I used the MSP430F135 (older device) I had problems
where if the pwr supply voltage did not go to zero when shut down and if there
was some capacitance still charged to about…
Hi Louis,
the lastest SW-version for MSP430-GANG ( http://focus.ti.com/docs/toolsw/folders/print/msp-gang430.html ) is V1.51!
This version has support for new devices: MSP430F5513, MSP430F5514, MSP430F5515, MSP430F5517, MSP430F5519, MSP430F5521, MSP430F5522…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
Hi Miles,
I recommend using the MSP430 product selector http://focus.ti.com/paramsearch/docs/parametricsearch.tsp?&familyId=342&uiTemplateId=PP-T-GSPA_T&techFamId=null&rootFamilyId=null§ionId=95&tabId=1200&appId=null&viewDeviceCallingPage=null&totalCount…