Part Number: MSP430G2332 Dear friends :
My problem is as followings:
Assembly program by IAR is work correctly. But, almost same Assembly program by CCS is not work as by IAR.
The IAR assembly program and CCS project fold are attached.
main.asm…
Part Number: MSP430G2332 I'm waiting on a custom prototype board that I designed that uses the MSP430G2332, and I'm trying to create the initial CCS project while I wait. I don't have a devkit. CCS11 is not showing MSP430G2332 as target option. I only…
Part Number: MSP430G2332 Hi Sir,
Our customer reported that MSP430G2332 cannot working normally after reset in low voltage. That is, after the MCU power off, the voltage of large capacitor drops to 1.5V and then power on again, there will be a phenomenon…
Part Number: MSP430G2332 We urgently need feedback on this complaint.
Product return: CPR221065501
At product returns no input and upload is possible
Error description
Freshly produced devices do not pass the function test. The function test…
Part Number: MSP430G2332 Hello,
Can TI provide a written document for the following questions in order to use it as a certificate of conformance for the ATEX certification.
The MSP430G2332IPW14R does not contain any voltage enhancement circuits…
Part Number: MSP430G2332 Other Parts Discussed in Thread: PMP4496 i have taken a power bank project from ti i have fabricated and assembled the pcb and also programmed it now i want to know how to use it i have connected a battery also its charging also…
Part Number: MSP430G2332-EP
I have a few questions about our production MSP430G2332-EP. I will use the part mentioned in my project in the field of aviation, but can you share with me the document showing the mtbf values of this part and which DAL…
Part Number: MSP430G2332 Hi,
I use the MSP430G2332 in a sounding application.
When I power my product on at 24V it starts sounding
When I send a pulse to 0V (200ms width) on the power supply. The sounder should reset.
When the pulse is over, some…
Part Number: MSP430G2332 Other Parts Discussed in Thread: ENERGIA , MSP-EXP430G2ET , , MSP430G2553 Tengo el MSP-EXP430G2ET utilizando el compilador ENERGIA con el MSP430g2332. Me sale un error que no tiene la serie MSP430G2xx2. Estoy utilizando la versión…
Part Number: MSP430G2332 Hi.
I have a query from a customer. They are currently using a MSP430G2332 for some visual alarm devices, combined to a 10 ppm crystal. The are testing the NDK NX3215SA ( https://www.ndk.com/en/products/search/crystal/1188854_1494…