Other Parts Discussed in Thread: MSP430G2352 customer said:
I'm having trouble deciphering the correct JTAG connections to use on the MSP430G2352 because the pin names of the part do not match the pin names referenced in application note SLAU278H.…
Hello I hope someone can provide help. I have a board (inserted inside a plastic/metallic box)
equipped with a MSP430G2352. The board is battery supplied with a CR2032 (like a sort of
remote control) and the cpu is always in LPM4 and wakes up with…
Other Parts Discussed in Thread: MSP430G2352 I am using CCS4.2 with the TI Launch Pad. I have been having an increasing amount of trouble getting the code to load into the target when I click on “debug active project”. It appears that as the…
Other Parts Discussed in Thread: MSP430G2211 , MSP430G2352 I am using CCS V4.3.4.00033 with the TI LaunchPad (MSP-EXP430G2). The LaunchPad shipps with an MSP430G2211. I ran the "blinking LED" code example, no problem. I added some additional code…
Other Parts Discussed in Thread: MSP430G2352 Hi all,
one of my customers is using the MSP430G2352 for an application and needs the MTBF data for the same.
can someone please point me to the data.
regards,
GJ
Can Launch Pad Dev Kit: MSP-EXP430G2, can be used to evaluate MSP430G2352, 20 pin package parts ? Or if any hardware modification is needed to do so?
regards
Other Parts Discussed in Thread: MSP430G2352 Hi all,
I am using ACLK from VLO for watchdog timer interrupt (BCSCTL3 = LFXT1S_2;), I want to know the frequency of that VLO clk and tolerance. My device is MSP430G2352. I searched in Datasheet but could not…
Other Parts Discussed in Thread: MSP430G2352 Hi,
I am using MSP430G2352. I want to know what are electrical charateristics of of I/O port when microcontroller is not powered up. I my circuit, before powering micro, i am supplying voltage less than 3.3V…
Other Parts Discussed in Thread: MSP430G2352 Jens,
Hi,
In my application i am measuring voltage using 10bit A/D across voltage divider over the temp range -20C to 70C. I want to know which tolerances i need to consider for A to D measurements apart from…
Other Parts Discussed in Thread: MSP430G2352 I'm very new to making devices using a MSP430. I'm making a pulse counter that displays the amount of voltage pulses sent across a MOSFET. I've already written the code to multiplex the signal across…