Part Number: MSP430G2403 Other Parts Discussed in Thread: UNIFLASH , Hi team,
I would like to be able to verify the checksum and I tried finding it in the GUI but cannot find it. I then found an old post online in the TI forum how to find it through…
Part Number: MSP430G2403 Hi team,
I have questions on power off sequence of MSP430G2403IPW28R.
- Do you have time limit to power off, like less than 10 ms?
- Do you have specific power off sequence, for example, power off after stopping main clock…
No, now I am not 100% sure (actually, don't remember) if I had wrong fuse check report for 2xx flash family, but I am sure that I have it for 5xx flash family (because I use it more frequently). There is no VPP and poly fuse with 5xx, but due to wrong…
I presume this .bin file is created by using either tiobj2bin or some variant of objcopy.
There is no industry standard format for a .bin file. objcopy started as a Unix utility. Here is the objcopy man page entry on a .bin file ...
When objcopy generates…
Part Number: MSP430G2403 Other Parts Discussed in Thread: MSP-FET , MSP430G2755 Tool/software: Code Composer Studio I developed a product using the MSP430G2403 using CCS4 on an XP machine. I'm trying to move it to CCS7 on a win 10 machine. CCS4 does not…
Part Number: MSP430G2403 Other Parts Discussed in Thread: MSP-EXP430FR2433 , ENERGYTRACE We are working with a small datalogger powered with a CR1216. We use an MSP-EXP430FR2433 Launchoad to measure consumption (powering the board with the launchpad)…
The problem was fixed when I removed the 1K pull-up resistors on the masters.
Not sure why the extra resistance between buffers was causing it to fail, but it works now.
Thanks for your help.
-Thomas
Hi All, First let me brief the background of my problem. I am working on a project , where I am collecting data from accelerometer via I2C, filtering the data and then performing calcuations over data. I have timestamped these individual operations and…
Nick Hazzard said: If the MCU is powered on I get about 26Ohm to GND on RX. I did a full erase and still get 26Ohm on RX, while every other pin measures in the 20MOhm range.
Try hold reset pin to gnd and measure again, if still persist low resistance…
Other Parts Discussed in Thread: MSP430G2403 I want to know if the MSP430G2403 is factory tested or guaranteed to operate off the DCO at 16 MHz at all four temperature and VCC corners. The spec sheet allows operation up to 16 MHz but over all temperature…