Part Number: MSP430G2755 Hi, Greetings. Our customer is looking for a target development board for MSP430G2755IRHA40R (40-pin) VQFN (RHA)). They would like to use it to program their chip. We've checked TI website and we've only find the MSP-TS43…
Part Number: MSP430G2755 Tool/software: Code Composer Studio Hi team,
During the installation of CCS V9.2 on the computer, the following problems are encountered. The error page is as follows. Please help to analyze the causes. Thank you!
Thanks and…
Part Number: MSP430G2755 Hi,
could you please help review below schematic? the application is 20s E-bike battery solution.
thanks and best regards,
Sophia
Part Number: MSP430G2755 Tool/software: Code Composer Studio For the same target board, some CCS projects can be burned, some CCS projects can not be burned.
Part Number: MSP430G2755 I believe I am seeing a variation of a timer period of 20% in the temperature range -40 deg C to 80 deg C. I have an ISR that raises an interrupt every 50ms on timer A1, the timer source is SMCLK which in turn is sourced from…
Part Number: MSP430G2755
Do the glue used to stick the die on the main frame in the ICs contain silver for conductivity purpose?
Is silver used for wire bonding?
BR
Anders Lange
Part Number: MSP430G2755 Hi MSP430 team.
Using the MSP430G2755, I am facing what looks to be a LFXT fault.
around 0.1% of the parts doesnt work, my best guess is that this is due to the XOSC5 errata.
Whats the recommandations for a workaround here?
The…
Part Number: MSP430G2755 Other Parts Discussed in Thread: CC1125 , , MSP430F5529 Hi MSP430 team.
The PCB is done with a CC1125 and the MSP430G2755.
I have noticed that a Sigfox demo is available for the MSP430F5529.
Is it possible to run the Sigfox code…
Part Number: MSP430G2755 Other Parts Discussed in Thread: CODECOMPOSER Tool/software: Code Composer Studio I've got new board in and I cannot get it CodeComposer to detect it. I'm jumping 3.3V on to the board, so the only parts populated are the JTAG…
Part Number: MSP430G2755 Hi,
I've inherited a problem project and don't have lots of MSP430 experience.
Looking through the datasheet I see there's an SPI baud rate pre-scaler UCAxBR0 and UCAxBR1 which form a 16 bit prescaler.
Question I have…