Part Number: MSP430G2955 Other Parts Discussed in Thread: ENERGIA , MSP-EXP430G2ET , , ENERGYTRACE Hi, I am trying to use MSP430G2955 on a custom board and MSP-EXP430G2ET LP to program it using SBW interface and Energia IDE. I can program the MSP430G2955…
Part Number: MSP430G2955
We are using time 1 TA1R with continuous mode for generating system ticks. Every time timer overflow interrupt occurs, we will increment a counter in firmware to track the upper 16 bit tick in the interrupt context
In order…
Part Number: MSP430G2955 Hi All,
I have msp430g2955 and I have implemented firmware that work as I2C slave mode with all things works fine like register set and get working fine..
Only issue that I am facing like on long run whitout accessing this…
Part Number: MSP430G2955 Tool/software: Hello there,
We need some assistance with one of our projects involving the MSP430G2955 microcontroller. We're currently using the device with a 1 MHz internal clock and testing it with a Burst Field Generator…
Part Number: MSP430G2955 Tool/software: Hi.
Does the MSP430G2955 support the blown fuse function? If yes, how to operate through the SBW interface? Please tell me which Windows software supports MSP430's blown fuse function, thank you!
Part Number: MSP430G2955 Tool/software: Hello, is there any reason why I can't use the Flash area 0x2100..0x21FF anymore? Used to be I always started code at 0x2100 . Now I had to change the linker setup to start Flash at 0x2200 ,which works.
I always…
Part Number: MSP430G2955 Other Parts Discussed in Thread: MSP430WARE Tool/software: I'm having an issue with getting my code working with CCS 12 vs CCS 8. I had to migrate as my Windows 7 machine isn't allowed on our network. I have no issues compiling…
Part Number: MSP430G2955 What is the minimum operating voltage level required to do flash operation in MSP430G2955?
What will happen if we do a Flash Write Operation when the input voltage is below Flash operating voltage?
What will happen if we do…
Part Number: MSP430G2955 Tool/software: I am relatively new to using CCS (v. 12.5.0.0007) for a MSP430 project.
In Debug mode I can pause the run and see values of the variables I want to see in the Expressions Window.
There is an option for Continuous…