Part Number: MSP430I2020 Hi Team,
Customer is requesting for TLP ESD performance and latch-up test report for MSP430I2020, can you help to provide them? Thanks a lot!
Part Number: MSP430I2020 Got into a bit of problem when using MSP430 Flasher to upgrade firmware in one of our products with the MSP430I2020 MCU.
When using the MSP430Flasher to upgrade firmware code, the INFO segment got erased and the factory calibration…
Part Number: MSP430I2020 Tool/software: Hi There,
I am new to E-metering, and having circuits reference neutral and/or earth.
When I look at tidu454a page 13, I see the MSP430I2020 also references neutral. Assuming the circuit is completely enclosed…
Part Number: MSP430I2020 Hi Team,
How to calibrate SD24?
TRM "The SUC should then calibrate the SD24 by writing the calibration value into the SD24TRIM register." How to determine calibration value?
In my opinion, When input is 0, the SD24MEMx…
Part Number: MSP430I2020 Hi Team,
My customer is use MSP430I2020 SD24 to weight detection, but the value is always jump.
Is it a normal phenomenon? How to optimize the program so that the ADC value is stable?
Thanks a lot!
Best Regards,
Z…
Part Number: MSP430I2020 Is there an automatic fallback path for VREF, if the VREF pin is configured as input (external) and the actual applied voltage is "0"?
Part Number: MSP430I2020 Other Parts Discussed in Thread: UNIFLASH , MSP430I2040 , CCSTUDIO , MSP-FET hello
i'm trying to flash an MSP430i2020 (and MSP430i2040) but keep getting 'verification failed' when flashing with ccstudio and uniflash * ccstudio…
Part Number: MSP430I2020 Hi TI team, This is regrading Single Phase Energy Meter Design with RS-485 communication. We are planning to use MSP430I2020 Metering MCU for the same.
I need your support in reviewing the neutral connection & Ground portion…
Part Number: MSP430I2020 Hi,
Could you tell me about the effective number of bits in MSP430I2020.
A resolution that can divide 10000 of Min 1g and Max 10000g is required.
Thanks,
Koki
Part Number: MSP430I2020 Hi,.
SMCLK = DCO/1
I output SMCLK to P1.1. And probe it. Its Freq=11.672MHz
But the spec should be 16.384MHz.
I need extra setup for it?