Part Number: MSP430I2021 Hi experts,
Let me check the setting of the EUSCI register (UCBRSx) in the following system.
SMCLK = 16.384MHz/4 = 4.096MHz N=4.096MHz/38400bps = 106.6666...
In the above case, which is correct?
Rounding up the decimal point: …
Part Number: MSP430I2021 Hi,
while giving heat to the device controller stops working, only core voltage is okay otherwise all peripherals stop working.
after reset in runtime also it's not okay, I have to on/off the whole device to make the controller…
Part Number: MSP430I2021 Other Parts Discussed in Thread: MSP-EXP430F5529LP Hello,
I'm trying to connect the MSP-EXP430F5529LP.
After programming MSP-EXP430F5529LP with the firmware TI_MSP_HIDBRIDGE__1_00_04_00__MSP-EXP430F5529LP.txt
I get No connected…
Part Number: MSP430I2021 Hello,
I am import a source code from EnergyMeasurementDesignCenterWorkspace for MSP430I2021 , when I compile this code in IAR than I got following error
Fatal Error[e59]: Module dc_filter16 ( C:\MSP430i2021 projects\lib\EM\IAR\MSP430i2xx…
Hi Leo,
Thank you for your support.
solved that with a change in settings while creating a .hex file.
Solution: In CCS V6.0 Hex utility settings specify RAM and Memory width only.
Part Number: MSP430I2021 Hello, customer want to use the MSP430i2021 in 110°C enviroment. He know that he is out of spec and TI can't garantee for anything. But he ask what the critical part would be at this temperature: package, digital or analog circuits…
Part Number: MSP430I2021 Hi experts,
Please let me check the RST/NMI/SBWTDIO pins.
Q1: Am I right in thinking that when the RST/NMI/SBWTDIO pin operates in reset mode (or NMI mode), it functions as an input and not as an output?
In general, I think the…
Part Number: MSP430I2021 Hi experts,
I would like to know about the fail-safe feature of MSP430I20xx.
As far as I can tell from "4.2.1.3 Fault Detection and Fail-Safe" in the user's guide, when using the external resistor mode, the DCO fault (For example…
Part Number: MSP430I2021 Hello
I'm trying to find documentation on the subject and I didn't find it, I'm afraid it doesn't exist and that's why I decided to ask here on the forum.
I need to analyze the Zero Crossing of the AC wave…