Part Number: ADC31JB68 Hi, the ADC31JB68 datasheet shows the baluns in the "current configuration mode" to convert the unbalanced to balanced signal in the analog input.
Is there any special requirement to use this structure of the baluns for…
Other Parts Discussed in Thread: TLV320AIC3262 hi,
in our design TLV320AIC3262 is connected to our SOC chip through 2 I2S interface(AS1 and AS2) and I2C, my questions are
1) The datasheet mentions 8se/ 4 diff inputs can be used as mics, does the two I2S…
Hi Damien,
DAMIEN CHARNAY said: I will be able to do this for you immediately tonight, it is complicated.
It doesn't have to be detailed. Just a high level overview of connections.
DAMIEN CHARNAY said: To enlighten you on my system it is a high power…
Part Number: CC1120 Hi Guys,
can somebody explain a purpose of IOCFG3 (2,1,0) - GPIO3 (2,1,0) Pin Configuration mode?
Is this an analog output (signal) before ADC?
We are looking solution where we can sample the IF I/Q signals by external ADCs.
I know…
Part Number: CC1310 Hi,
I'm developing for a CC1310 and I'd like my application to control which analog input pins are used by the sensor controller rather than configuring statically in sensor controller studio. Is the following the best way to do that…
Hi Francois,
I am unaware of any code library for MSPM0 to get the angle from an analog sensor's data. This seems dependent on the sensor's data format/output range and shouldn't be too complicated. We do have a MATHACL which can assist if needing to…
Part Number: ADS131M06 Other Parts Discussed in Thread: ADS124S08 Hello Guys,
Good day.
Our customer is designing a board that requires 12 ADC channels, 6 are differential and 6 are single ended. Can the ADS131M06 be configured to support the 6 single…
Hi
Please refer to 5.4 Write Protection section on MSPM0 C-Series 24-MHz Microcontrollers Technical Reference Manual (Rev. A)
flash Static Write Protection can is configured on NONMAIN
Dynamic Write Protection can be found on flash operation code example…
Hi Munan,
I checked the internal data base. However, there is no related information for DMA module in it.
I more thing I noticed that the DMA in MSPM0 only works in PD1 and sourced from MCLK. There will not be this much configurations as the MSP430 device…
Part Number: MSPM0G3107 Tool/software: Currently, we use MSPM0 SDK v2.1.0.03 to build our FreeRTOS codebase. We would like to modify the SDK. How can we configure it step-by-step in CCS IDE?