Part Number: MSPM0-DIAGNOSTIC-LIB Tool/software: Hi,
I'd like to utilize the MSPM0 Diagnostic Library 1.0.0.xx or above to integrate selftests required by the certification.
I requested on through this page: MSPM0-DIAGNOSTIC-LIB earlier but the version…
Hi Lee,
Kyungjae Lee said: Question 1: RAM Test
1. Yes, the size is depends on customer selection.
2. Yes, user should creat the related memory section in cmd, our example project should give a good example.
Kyungjae Lee said: Question 2: FLASH…
Part Number: MSPM0G3507 Tool/software: Hi, Can anyone help me to grant access for this file? I'm gonna use this microcontroller for my BMS project. Thank you
Hi Pengfei,
From customer:
"
MSPM0 Diagnostics Library 0.90.00.01 released on August 04, 2023
MSPM0 SDK 2.04.00.06
TI ARM Clang 4.0.2.LTS
Build does not use Composer Studio but rather CLI with options from the library documentation.
…
Part Number: TMS320F28P650DH Other Parts Discussed in Thread: C2000-SAFETI-DIAGNOSTICS-LIB , C2000WARE Hi Experts,
What's the self diagnositcs coverage of C2000-SAFETI-DIAGNOSTICS-LIB?
Customer need to input this information to TUV, We are looking…
Part Number: C2000-SAFETI-DIAGNOSTICS-LIB Tool/software: Hello,
We will beginning a project soon and will likely need support down the road. For confidentiality reasons we would like to set up an email relationship if at all possible. Is this something…
Part Number: MSPM0G1107 Tool/software: Hello all,
I reported a missing function in the driver lib half a year ago ( link ). I checked in sdk version 2.03.00.07 which was released recently, but I still did not find the needed function. Since the SDK…
Part Number: C2000-SAFETI-DIAGNOSTICS-LIB Other Parts Discussed in Thread: C2000WARE
Tool/software:
How can I use the C2000-SAFETI-DIAGNOSTICS-LIB in an EABI project when existing .lib files are COFF ABI?
Part Number: TMS320F28388D Other Parts Discussed in Thread: C2000-SAFETI-DIAGNOSTICS-LIB , C2000WARE Tool/software: hello there
i want to porting
C2000-SAFETI-DIAGNOSTICS-LIB
are there any documentation illustrate how could i do that ??
Part Number: MSPM0G1107 Other Parts Discussed in Thread: DRV8313 Tool/software: Hi all,
for our application we use TIMA0 to control the external motor driver DRV8313.
The PWM inputs of the motor driver are connected to the CC outputs of the MCU and…