Part Number: MSPM0C1103 Hi srs,
We are using the MSPM0C1103 microcontroller to read two ADC ports. However, we have identified an operational stability issue. In a batch of 200 units, 60% function correctly, while 40% experience an application freeze…
Part Number: MSPM0C1103 Other Parts Discussed in Thread: SYSCONFIG
Toolchain/IDE: Code Composer Studio / SysConfig
Hi TI Team,
I am experiencing an issue with ADC12 sequence conversion on the MSPM0C1103 across multiple boards running the exact same…
Part Number: MSPM0C1103 Dear Team,
On the figure, I think that the red timing is BOR status.
Is my understanding correct?
Best Regards,
Seijiro Matsuoka
Part Number: MSPM0C1103 Hi All,
I download the mspm0_sdk_2_11_00_07.zip file ,i would program on keil, but i didn't has any sample code about prgram flow operate. there is only empty.c (empty main function), may i have the sample code with all memory…
Part Number: MSPM0C1103
My GPIO pin PA0 on MSPM0C1103 is set low no matter what I try. I have attached my project.
I have tried 3 different boards. The connections between the controller and my point of measurement are fine. I can detect input if…
Part Number: MSPM0C1103 Tool/software: Good morning TI team
I am using MSPM0C1103 micro-controller with the following setup: IAR Embedded Workbench IDE and J-link (by SEGGEER).
In MSPM0C1103 there is a Cortex M0+:
I need to know if it’s possible…
Part Number: MSPM0-SDK Other Parts Discussed in Thread: MSPM0C1103 , SYSCONFIG I am using CCS12 Version: 12.8.1.00005
I am using the MSPS003F3 variant of the MSPM0C1103 and cannot select resistor pullup under the Digital IOMUX features for an input…
Part Number: MSPM0C1103 Other Parts Discussed in Thread: MSPM0C1104 Good afternoon TI team
I’m developing a new design using the following uC: MSPM0C1103
In a TI example of sdk\LP_MSPM0C1104 (adc12_single_conversion), it’s possible to see the offset…
Part Number: MSPM0C1103-Q1 Tool/software: I would like to know if the MSPM0C1103-Q1 chip supports software shutdown to enter shutdown mode, and if it can share the same power supply with other chips. I look forward to your reply. Thank you very much.
Part Number: MSPM0C1103 Tool/software: Good morning TI team
In my project, I am using MSPM0C1103 micro-controller with the following setup:
IAR Embedded Workbench IDE;
J-link (by SEGGEER);
In the production software version, I had to enable…