Part Number: MSPM0C1103 Tool/software: Hi,
I would like to program/debug the MCU target MSPM0C1103SRUKR by the XDS110 tool via the SWD pins.
Which minimum pins (of the SWD) do I need to connect between the XDS110 debug port and the MCU target MSPM0C1103…
Part Number: MSPM0C1103
Tool/software:
HI TI Champs
We are happy to announce the release of our 1$ ARM board powered by MSPM0C1103 from Texas Instruments. Entire design is open source, released in the github. github.com/.../1$ ARM board Board Features …
Part Number: MSPM0C1103 Other Parts Discussed in Thread: MSPM0C1104 , SYSCONFIG Tool/software: I am using CCS 12.8.1 and have created an 'empty_mspm0c1103_nortos_gss' project.
When I try to configure an output pin, the IDE thinks that I am using…
Part Number: MSPM0C1103 Tool/software: Hi,
We are considering a solution that uses MSPM0 to sense the coil current and perform current feedback control.
The input to MSPM0 is the current command value (analog) and current feedback (analog).
The output…
Part Number: MSPM0C1103 Tool/software: Dear TI,
I would like to create a new CCS project for a MSPM0C1103 microcontroller, but the device is not available in the list of devices. I have installed the MSPM0 series on my CCS (version 12.4.0, installed…
I am testing through the LP-MSPM0C1104 EVB. LP-MSPM0C1104 I am having this problem. not 1103. I opened the wrong subject name.
I see that MSPM0C1104 does not support BSL. When I look at the pin configuration I see that CCS does not support BSL for MSPm0c1104…
Hello Che Wen Yeh,
The MSPM0C1104/3 family is a good choice as it has the ability to drive the LED segments using standard GPIO pins. Do we know how many LED segments there are?
The MSPM0C's ADC can be used for monitoring voltage and current detection…
Part Number: MSPM0C1103 Tool/software: hi,
I USED THE SWIO AND CLK PINS AS IO PINS IN MSPM0 AND NOW I'M HAVING PROBLEMS WITH THE DEBUG PART HOW CAN I DEBUG THIS WAY
best regards
Part Number: MSPM0C1103 Tool/software: Hi,
can you please help me to interpret the endurance numbers of the flash memory especially the term "NE(MAX)"?
Does it mean that each flash cell can be erased 802 000 times before it is permamently…
Part Number: MSPM0C1103 Tool/software: Hi,,
Do you have periodic debbuggin in CCS theia? When I press start, I want to see the variable on the Watch screen change instantly while in debug.
The variable changes by pressing Stop Start, but I don't want…