Part Number: MSPM0C1104 Tool/software: MSP team,
The datasheet for MSPM0C1104 does not have any pins labelled as BSL_invoke, BSLSDA, BSLSCL. Which pins should be used for the BSL?
Can you confirm that this device does in fact come loaded with the BSL…
Part Number: MSPM0C1104 Tool/software: Hi Expert,
msp sdk: mspm0_sdk_2_02_00_05
CCS: 12.8
i just build and run the debug for the example " adc12_triggered_by_timer_event_LP_MSPM0C1104_nortos_ticlang".
The program stops at below.
__STATIC_INLINE…
Part Number: LP-MSPM0C1104 Tool/software: Hi, I found below example project in SDK 2.02.00.05. https://dev.ti.com/tirex/explore/node?node=A__AKiw9xaBn-Aakb2oWVMG5g__MSPM0-SDK__a3PaaoK__LATEST In readme file, there is a link to app note, but the link is…
Part Number: TMS320F2800132 Other Parts Discussed in Thread: MSPM0C1104 ,
Tool/software:
Hello Team,
Does the MSPM0C1104 support ECC RAM testing, and is there any example code in the SDK for this
Hello Santhosh,
1). Stack is a part of SARM which is the bottom of SRAM. If you want to store data in stack directly, you can try to use the pointer which I have mentioned before.
2). But why you want to store a permanent value in stack directly? Stack…
Part Number: MSPM0C1104 Other Parts Discussed in Thread: SYSCONFIG Tool/software: I'm using MSPM0C0114 in SOT-8 package. Therefore, not all IO pins from the die (I assume that all different packages contain the same die) are connected to the package pins…
Part Number: LP-MSPM0C1104 Other Parts Discussed in Thread: MSPM0C1104 Tool/software: I’m considering using the MSPM0C1104 microcontroller for a project and I have a few specifications in mind:
I want to implement a feature where an output is triggered…