Part Number: MSPM0G1505 I want to achieve a function based on input capture, first of all, it is necessary to capture both sides of the edge, the duty cycle and period of the first edge should be recorded, but it is necessary to record the value of both…
Part Number: MSPM0G1505 Hi team
Currently, my customer uses some motors are equipped with a function to detect the inflow current of the driver. The chopping component is cut at high frequency with a CR filter, and then amplified with an AMP Input…
Part Number: MSPM0G1505 Tool/software: Hello,
In the datasheet we specify an ODIO low level input voltage, and an "all IO except ODIO and Reset" low level input voltage:
But then what is the low level input voltage level for the reset signal?
…
Part Number: MSPM0G1507 Other Parts Discussed in Thread: MSPM0G3507 ,
Hi experts,
I understand from the original thread that there is an issue. As an alternative solution, is the following method correct?
Import "empty_lp_mspm0g3507_nortos_ticlang…
Part Number: MSPM0G1505 I Use the compare mode example, the sys set rising and falling mode, but it can‘ enter the “cc0_UP”, and thepwmPeriod_1 =0 all the time.
I only want to achive the two edge(rising and falling) ,read the counter value.
…
Part Number: MSPM0G1505 Other Parts Discussed in Thread: MSPM0L1303 , SYSCONFIG Tool/software: Hi We need to upgrade from MSPM0L1303 to MSPM0G1505 (VQFN24), and we can ' t change the layout. We are using 1.4V internal Vref, MSPM0L1303 don't need any external…
Part Number: MSPM0G1505 Other Parts Discussed in Thread: UNIFLASH Tool/software: Hi team,
My customer is development M0G1505. They report below problem. Please help clarify. Thank you.
Problem description:
They use BSL to update M0G1505 FW. However…
Part Number: MSPM0G1505 Other Parts Discussed in Thread: MSPM0L1303 , SYSCONFIG Tool/software: I am migrating a project from MSPM0L1303 to MSPM0G1505.
When I am recreating the configuration using SysConfig I get an error as soon as I select "Channel…