Part Number: MSPM0L1106 Tool/software: Hello,
I had a customer who's using both the XDS110 and J-Link debuggers to develop their application. One thing they've noticed is that the same code which works on J-Link doesn't work with the XDS110. Neither…
Part Number: MSPM0L1106 Other Parts Discussed in Thread: SYSCONFIG Tool/software: I am encountering a problem where the pin state read via the “DL_GPIO_readPins” API does not match the actual pin state. I initially configure the pin as an output, then…
Part Number: MSPM0L1106 Other Parts Discussed in Thread: LP-MSPM0L1306 Hello I would like to operate a MSPM0L1106 (SOT-23-THN (DYY)) on a SOT23-16 breakout board as a target on a LP-MSPM0L1306 LaunchPad. On the breakout board, all 16 pins are directly…
Part Number: MSPM0L1106 Hi MSPM0 champs,
We would have specific questions about the SPI module behavior on MSPM0L11xx :
Q1/ When sending 8-bit data to the SPI Tx buffer, is the response stored in the Rx buffer?
Q2/ What happens if the received response…
Part Number: MSPM0L1106 Other Parts Discussed in Thread: MSPM0L1306 Tool/software: Team, Can you please confirm the below? We want to use the internal bootloader of an MSPM0 to load our application via the internal UART later in production: Refering to …
Part Number: MSPM0L1106 Tool/software: Hi,
Started a project for MSPM0L1106 based on the empty cpp project in driver lib examples.
Added blinking LED in the loop with a delay and that works fine.
Wanted to use the SysTick_Handler to generate a 1ms interrupt…
Part Number: MSPM0L1106 Other Parts Discussed in Thread: SYSCONFIG Hi,
Using the PICO pin as a single pin communication for data to a WS2812B LED via DMA.
How do I only configure PA18 as PICO and the other SPI pins as GPIO?
This is not possible in SYSCONFIG…
Part Number: MSPM0L1106 Other Parts Discussed in Thread: SYSCONFIG , MSPM0L1306 Im trying to configure pin 26(PA22) & pin 28(PA24) of MSPM0l1106 MCU as analog input from syscfg but the cmpiler is only showing ADC0.
Part Number: MSPM0L1106 Hello,
During our developing for MSPM0L1106 programmer. when I using BSL Command of Factory Reset(80 01 00 30 DE 20 24 0B), after command is executed, the chip couldn't be connected again wher using SWD or BSL, Why?
Also,…
Part Number: MSPM0L1106 Dear Sir/Mrs.
We are MCU Programmer developer and supplier.
During our developing for MSPM0Lxx Chips, we foud that once we write data(this data is disorder, just for testing, not arm instructions) to chip flash, after poweron…