Part Number: MSPM0L1227-Q1 Other Parts Discussed in Thread: MSPM0L1227 Tool/software:
Dear team,
to meet the ASIL requirements of our project, we need to enable the CRC feature in the TLIN1431, which is configured to communicate with the MSPM0L1227…
Part Number: MSPM0L1227-Q1 Tool/software: Hi Champs,
Do we have 24pin VQFN package information as below? I found several other packages in the datasheet, but no 24-pin package.
I also find a file but there is no detail information
https://www…
Part Number: MSPM0L1227-Q1 Tool/software: Hi,
I wonder whats the range of pullup- and pulldown-resistance for GPIOs is.
In the datasheet SLASFB5A, november 2024 page 52, only the typical value of 40kOhm is listed.
Part Number: MSPM0L1227-Q1 Tool/software:
Once a board fails to connect when debugging, the following error keeps appearing regardless of whether it is connected via the 10-pin DAP connector or the 2-pin SWDIO/SWCLK connector.
Also tried performing…
Part Number: MSPM0L1227-Q1
Tool/software:
Hi Experts.
Regarding TRM of MSPM0 L-Series 32MHz Microcontrollers.
Both 0 and 1 mentioned enableed. Is 0 disable?
Best regards,
Ito
( 93d3848a-5635-4363-aaf2-23fdadfa3fb9)
Part Number: MSPM0L1227-Q1 Tool/software: Hi MSP experts,
what is the maximum Interrupt latency of the MSPM0L1227Q1 meassured in CPU cycles?
Thank you,
Marinus
Part Number: MSPM0L1227-Q1 Tool/software: Dear team,
I am performing flash read at Address "0x0001F000" as below. Write opration is successful and I can see the intended data in memory window.
Code snippet from write API,
DL_FlashCTL_executeClearStatus…
Part Number: MSPM0L1227-Q1
Tool/software:
Hi Experts.
It seems that UDIV explanation is missing in MSPM0 L-Series 32MHz Microcontrollers.
But there is UDIV block is existing in following Figure 2-7. MSPM0Lxx Top Level Clock Tree.
How should…