Dan,
Are you able to provide a timeline of events? When was the EVM purchased? From what I can see they started a thread to work on the EVM about two months ago, we went back and forth several times and the SW was eventually delivered after 45 days. It…
Part Number: TDA4VM
Tool/software: TDA4SW0804/pdk_08_04_00_21
hi Ti,
we found that when we send PTP messages, the following log errors occasionally occur: "CpswCpts_ioctl: Eth TX event not found (msgType=0, seqId=16, dom=0, portNum=1)";
This…
1. We tried with both VCC1 powered up and with VCC1 powered down and noticed the same behavior
2. We did not try reading any faults with SPI, but did see that nFLT1 was active (when VCC1 was powered up)
3. The test was a clean power up. We tried:
* VCC1…
Well, adding this line at the end of GATT_EventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData) function solves the heap problem above.
GATT_bm_free(&(gattMsg->msg), gattMsg->method);
I wonder why it is not there by default in the SDK original…
Part Number: TMS320F28075 Other Parts Discussed in Thread: C2000WARE Tool/software: Dear Experts,
When we were debugging SPI, the RXBUFF register value kept reading 0xff.It seems that the data was not received. At this time, there is data on the SPI bus…
BLEAppUtil_getSelfEntity(); did the trick. I spent some time trying to grab the correct task ID and that was exactly the function I was in need.
Now the events are happening and that makes all sense in the end.
I was in doubt since the header for GATT_EventHandler…
Part Number: TDA4VH-Q1 Other Parts Discussed in Thread: TDA4VH Tool/software: Hello,
We are experiencing an issue where the TDA4VH is not receiving images from the camera. This problem doesn't happen a lot, maybe 3-4 times out of around 200 power cycles…
Part Number: DCA1000EVM Other Parts Discussed in Thread: IWR6843ISK-ODS , IWR6843 Hello,
I'm trying to use DCA1000 with IWR6843ISK-ODS board to do some raw data captures.
I just installed mmWaveStudio and all the dependencies. I had set up the jumpers…
Part Number: IWR1443BOOST Other Parts Discussed in Thread: IWR1443 , UNIFLASH Hi Team, Asking for your assistance on our customer's query concerning the use of mmWave studio. They're currently using DCA1000EMV with IWR1443BOOST. When using mmWave studio…
Part Number: AWR1243BOOST Other Parts Discussed in Thread: AWR1243 I am using mmWaveStudio to interface with the AWR1243BOOST. The BSS firmware used is C:\ti\mmwave_studio_02_01_01_00\rf_eval_firmware\masterss\xwr12xx_xwr14xx_masterss.bin, and the MSS…