Other Parts Discussed in Thread: AM1802 Hi,
I have a AM1802 target board using SPI1 FLASH boot. I have set the boot mode pins as SPI1 FLASH mode, and the board was used to be booted successfully. Then I measured the SPI pins, OSCIN, OSCOUT, and boot…
Part Number: LINUXSDK-OMAPL138 Other Parts Discussed in Thread: OMAPL138 Tool/software: Linux Hi,
TI, I am working on the usb2.0 port of omapl138,using the kernel linux-3.3 from da850-03.22.00.06 branch.
There is a 4G module ME3630 connect to usb2…
Part Number: AM1705 Tool/software: Linux
Hi ,
We are using AM1705 with SPI flash as SPI boot and XDS100V2 for programming.
We are not able to proceed further due to following issues:-
When we try to download ramdisk image ( ram_1 ) into…
Other Parts Discussed in Thread: OMAPL138 Hi,
I need to do shared resource managment between the two cores on the omapl138 (no linux and no Dspbios environment)
and I'd like to know if there is any kind of atomic read-modify-write opcode available…
Thanks for the reply Gil.
Now I am able to compile the codec engine examples. And I am not using and DVSDK or EZSDK, I have separately installed it.
But please suggest me one more thing as I have compiled the codec engine example and it is tested…
Part Number: OMAPL138B-EP Tool/software: TI C/C++ Compiler Some common utility functions need to be deprecated like this:
__attribute__((deprecated)) void TestDeprecatedMethod(int a, float b);
This works as expected on the ARM side of the OMAP like…
Other Parts Discussed in Thread: OMAPL138 Hello all,
I am using LogicPD's evmomapl138, ccs v5, sys/bios 6.33.1.25, nsp 1.10.0.03, and ndk 2.20.6.35.
I've ran the helloWorld example using DHCP and it has worked correctly. I've modified the code to…
Part Number: TMDSLCDK6748 Hello Ti team,
I am trying to find the pin-outs for the peripherals i want to use using the hardware schematics file found under revision A7a.
The peripheral i want to use is the Upp. Both channels. The J16 and LCD peripherals…
Hello.
Android: 4.2.1
Kernel: 2.6.32 (FROM SEMC Sony....)
Wifi/BT/FM: in JB4.1 used wl12xx.ko and wl12xx_sdio.ko and works everything.
History:
As You know in JB4.2 bluez was removed and Google add Bro..com Bluedroid stack.
Wifi working…
Part Number: BIOSLINUXMCSDK Other Parts Discussed in Thread: OMAPL138 I'm starting with the OMAP L-138 LCDK configuration files in the BIOSLINUXMCSDK for a custom board that is similar, but uses UART0 for the console and has no EMAC. I want to switch…