Part Number: PROCESSOR-SDK-OMAPL138 Other Parts Discussed in Thread: OMAPL138 , TPS2042B I have a 3 part question.
1. How do I interact with the mass storage device using the USB host controller? The documentation seems to indicate that the UART port…
Other Parts Discussed in Thread: AM3517 , WL1271 , OMAP3530 I am using AM3517 SOM-M2 ,it can realize bluetooth function,but i find friends in the forums are talking wl1271....,so i do not know whether it is what i want ,because AM3517 SOM-M2 has LBEH19XMMC…
hi,
I want to use system analyzer in my sys/bios project. I added UIA component "LoggingSetup" and remove LoggerBuf as the system analyzer user manual required(doc SPRUH43E) as bellow:
but when I run the project, I can see nothing logged in the…
Other Parts Discussed in Thread: WL1271 I am researching an issue with bluetooth usable distance with cyanogenmod7 running on a B&N Color Nook. The version of android is 2.3.5 running kernel 2.6.32.9.
The issue that I am experiencing is that bluetooth…
Hi, I want to use USB 2.0 hi-speed Host on my AM1808 to get snap shots from 5M USB camera. when i connect my USB camera interface to USB 1.1 host port, the driver found itseems and created the node as /dev/video0. But when i am trying to capture the sanpshots…
Part Number: TMDSLCDK138 Tool/software: Code Composer Studio Hi,
Project Hello on LCDKOMAPL138 board with XDS110 emulator, while going to debug, it generate an Error as follows:
Error connecting to the target: (Error -261 @ 0x0) Invalid response was…
Hello. I am using USB as device only mode operation. I have pulled up USB0_VBUS pin to 5V with an external 1K ohm resistor. I would not like it(USB0_VBUS) to connect to VBUS of USB connector for ESD.
Is this allowed ?(Does USB operate correctly?) …
Other Parts Discussed in Thread: WL1281 , WL1271 , WL1837 Hi All, Looking for help with a Bluetooth LE and WiFi coexistence problem I'm seeing with the TI WL1271L. I can use WiFi by itself fine and see 20-40 Mb/s when testing with iperf. I can connect…
Part Number: AM1705
Tool/software: Linux
hello,
I made a custom board which runs on the AM1705 processor. so far everything works fine. the only issues I'm getting are regarding external interfacing like UART, ETHERNET, and SD-CARD at OS level.…
Other Parts Discussed in Thread: SYSBIOS Hello,
I'm looking for information on how the synchronization of power management between ARM (Linux) and DSP (DSP/BIOS) works. Meaning, by changing the common resources in one processor what will happen with…