All,
This is a very helpful site to help you with Hardware Schematic Review for your designs using the OMAP-L13x/C674x/ AM1x family of devices. http://processors.wiki.ti.com/index.php/OMAP-L13x_/_C674x_/_AM1x_Schematic_Review_Checklist
Part Number: PROCESSOR-SDK-OMAPL138 I have been trying to include the Ipc library in a dsp project. It is kind of irriating becuase includes folder I can see the /home/local/ti/ipc_3_46_00_02/packages folder but for some reason when I do the #include…
Other Parts Discussed in Thread: AM3517 1 hciattach -t 50 /dev/ttyS1 texas 3000000
Found a Texas Instruments' chip!
Firmware file : /lib/firmware/TIInit_7.2.31.bts
Loaded BTS script version 1
texas: changing baud rate to 3000000, flow control…
Hello,
I need to establish one way SPI connection for communication between c6748 lcdk and AD5932.
In my code I use drivers, examples and h-files from C6748_StarterWare_1_20_03_03.
I wanted to varify the frequency of SPI0_CLK on oscilloscope, but…
Other Parts Discussed in Thread: OMAPL138 Hi,
I'm recently use DSPLINK to implement the communication between the two CPUs of OMAPL138,I need to tranfer data from dsp to arm twice one time ,but I only allocate only one buffer from the POOL,this is…
Hi,
I am working on AM1808 processor, I used NAND flash in our design which is micron 2Gb part:MT29F2G08ABAEAWP-IT:E TR Also i am using SPI flash in my design. I would like to use NAND flash for only my root filesystem. Can i have steps how to convert…
Hi Todd,
I was able to successfully run the MessageQ example for 6678 .Based on that example only tried i created my own project in CCS.
Regards,
Harikrishna
Hi,
The Uart 2 TX pin is toggling after reset but on the Hyper Terminal which is configured for 115200 baud rate garbage value appears. But according to the startup guide "BOOTME" string should appear on Hyper Terminal configured for 115200 after reset…
Other Parts Discussed in Thread: OMAP3530 Hello Everybody,
We have a our own USB based client device. We have developed the driver and the Application for Windows XP.
We would like to develop USB based driver on Windows CE 6.0, eairler we had bought…