Part Number: OMAP3503 Tool/software: Code Composer Studio Customer is using OMAP4430 and asked: Is the CCS (Windows version) able to cross compile (and configure) an embedded Linux (like Buildroot or Yocto)?
Regards, Bernd
Part Number: OMAP3503 Tool/software: Starterware Hello,
Is there any where we can find sdma driver (for any TI's chip) ?
I see edma, but not sdma.
Even if it's not starterware it can help.
Thank you,
Ran
Our problem was with the AM335x which is very similar to the OMAP3503. Turns out all the filter caps for the power supplies where assembled incorrectly so there was a large voltage ripple causing the processor to hang.
Part Number: OMAP3503 Tool/software: Linux Hi,
0 down vote favorite
I have a ARM OMAP based embedded system with 1 GHZ processor running Linux 2.6.33 cross compiled as CONFIG_PREEMPT. One of the Processes (process 1) is critical and need to run…
Other Parts Discussed in Thread: OMAP3503 , LINUXDVSDK-DM37X Hi,
I am using overo gumstix board which is based on OMAP3503 processor. I am using Linux kernel 2.6.32 on this board since 2010 and I want to upgrade the kernel source on this board.
Can you…
Hi,
My board boots up from SD card, I often see SD card corruption issue on Linux 2.6.32 kernel with omap3503 processor, this will create problem on boot up or on some applications to run due to some file corruption.
What you have done before corruption…
Other Parts Discussed in Thread: SYSBIOS , OMAP3530 Good afternoon,
I am having issues reading/writing from the flash in our application because the SYS/BIOS seems to setup the MMU in a way that makes these registers inaccessible.
I have read a few other…
Other Parts Discussed in Thread: OMAP3503 , TUSB1210 Hello,
I have a problem to configure an usbhost port of the omap3503
I have connected an USB3317 the the USBhost1 port of the omap3503. The pin CLKOUT (60MHz clock) of the USB3317 it is connected the…
Hi Kevin,
Looks like I am having the same issue with THS7303, could you please advice what was root couse in your case and how you fix it?
Thanks,
Kirill