Hi Team,
Customer has an issue with plug and unplug of USB device. Can you please help here if this is a known issue and any options to root cause and resolve this?
issue:
When ever there is a frequent plug in & plug out of USB serial devices such as …
Hello to All;
Have you people got solved this issue, detecting emmc on mmc2 interface?
And one more, wheather it works fine , if we connect to mmc1?
We will boot from nand, so that the emmc connected on mmc1 should mount automatically know?
Regards,
…
Hi Akshay
Sorry, I don't think I can help you this time.
I don't think I've come across this problem, and I've
already posted all relevant sourse code.
Hope you find a solution anyway !
Best regards
Jens
Other Parts Discussed in Thread: AM3703 We are upgrading our design from a OMAP3505 to a AM3703. We need to keep the S/W common between the 2 processor. In the MIDR register, is the Variant Field adequite to distingish between the 2 processors? The variant…
Just noticed that by letting MPU watchdog reset happen to generate a global warm reset, the data pins (dat7 e.g.) was driven to high (1.8v) slowly.
Anybody has an idea?
Thanks,
Philip
Other Parts Discussed in Thread: AM3703 , AM3715 Hi Forums,
I was looking at the data sheets for the OMAP 3503 and AM 3703 CPU's and I noticed that the signals for HSUSB2_CLK are dedicated for external transceivers 60-MHz clock inputs on the PHY. …
Other Parts Discussed in Thread: OMAP3503 Hello OMAP Team,
We have an MT9P031 sensor connected to the GUMSTIX OMAP3503 and experience video artifacts above 48MHz PIXCLK. The sensor uses a 24MHz from the uP and the PLL code and sensor setup have been checked…
When using the OMAP3503DCBB
We first boot an OMAP in UART boot mode, the OMAP transmits a few ascii characters to tell the loader software on the terminal end when it is ready. We usually see something like a 40W or a 40T depending on the version of…
Other Parts Discussed in Thread: DM3730 Hi,
I trying to use DVI output instead of LCD for OMAP3503 board. I've read instruction in VAR_OM35xx_P.bat and I've found out this: REM Note that if this variable is changed, a XLDR/EBOOT update are required…
Other Parts Discussed in Thread: OMAP3503 Hi,
We are using OMAP3503 processor on our board, which currently has SD Card interface.
We plan to use micro SD Card. Does OMAP3503 support micro SD interface?
Thanks,
Sanjeev