I have now sucess with communication to both IC's. I have changed two things.
First I checked, if I was right in remembering that the Göpel system access TRST and then a soft reset by sending 18 clocks onTCK, I was wrong, Göpel send 18 clocks…
Other Parts Discussed in Thread: OMAP3503 , OMAP3530 Hi.
I build WinCE 6.0 image with Silverlight(SYSGEN_XAML_RUNTIME) and DirectDraw(SYSGEN_DDRAW) support.
Image build with flags BSP_XRPLUGIN_DDRAW and SYSGEN_SAMPLEXAMLPERF also.
When i try to start…
Other Parts Discussed in Thread: OMAP3503 Hi All,
I am having a problem with my OMAP3503 based board. I am not able to flash the bootloader using EVMFlash tool. A popup saying "Failed to connect to the traget" is shown. The details are given…
Hi James,
Thanks for sharing the USB trace data. It will take some time for me to verify this.
Meanwhile, I was just going through the errata (TI document # sprz278f) and came across the Advisory 3.1.1.195 " HSUSB Interoperability Issue With SMSC…
Other Parts Discussed in Thread: OMAP3503 I'm working with a design which may potentially connect many devices to the GPMC bus on the OMAP3503. To make sure the processor can handle this design I'm looking through the 3503 data sheet trying to learn what…
Other Parts Discussed in Thread: OMAP3503 , TPS650731 Hi All,
We are facing a very strange issue on my OMAP3503 based issue.
We are using OMAP3503 CBC package and TPS650731 PMIC. And LDO2 of this chip is used to supply the power to OMAP VDDS_MMC1 domain…
Hello Greg,
While debugging winCE
fmd driver, I have found the
problem that were preventing my board to successfully boot.
The Onfi driver from
flasher is not programmed to properly configure de GPMC bus, this should be
done by platform configuration…
Other Parts Discussed in Thread: OMAP3503 , OMAP3530 Hi,
Custom Board with OMAP3503 Processor.
In the bring up level we are trying to draw few colors on the display like red,green.etc to check the RGB data lines of the DSS interface.
With this setup…
Hi ArunRM,
I am having similar issues, the slave device got unexpected value after long hours of running. The I2C2 controller intermittently reports NACK and AL errors, and leaves incomplete transactions. Have you found a solution to your problem? …