Dear all,
I would like to compiler power sgx driver for my card with 3515 processor, unfortunately some errors that I can't fix its. Somebody can help me.
I have used a kernel version 2.6.33.7 with somme driver modify and uImage run.
Thank you…
Other Parts Discussed in Thread: OMAP3515 Hi !
I am using a OMAP3515 with the 256MB SDRAM. It is working fine. However, for future support, we have to double the size of the SDRAM. We changed the x-loader and uboot. After the changes, we can access…
Other Parts Discussed in Thread: AM3715 We need a solution for the OMAP speed detection bug. One way is use an Onboard USB-hub. But that is not very clever. What is with the shinked OMAP version AM3715. Could that a replacement?
In the migration guide…
Other Parts Discussed in Thread: OMAP3515 , SYSCONFIG Hi,
I am running Windows CE 6 (based on 6.13 BSP) on an OMAP3515 ES3.1. I have configured the chip to go into OSWR on suspend. While looking at a suspend/resume issues I noticed that the core domain…
I'm missing something.
I have a new, custom board featuring the 3515. I am able to boot via UART3 and load u-boot. When I load code in this manner, I can use my JTAG debugger and view UART3 address space at 0x49020000. If I reset the board, load…
Other Parts Discussed in Thread: TPS65930 , OMAP3515 , TPS65950 Hi,
could you please give the min, typ and max TPS65930's current consumption when OMAP3515 in suspend-to-RAM mode?
Thanks.
Other Parts Discussed in Thread: OMAP3515 Hi all,
I am planning to port the camera driver of OMAP3430 processor to the OMAP3515 processor.
Is there any additional functionalities added on the OMAP3515 camera ISP other than which is found on the OMAP3430…
Other Parts Discussed in Thread: OMAP3515 , TPS65930 I design a industrial PDA use the OMAP3515 . I use the MMC1_DAT0~DAT3 as the SD card interface, GPIO128 ( N20 )configure as GPIO,read the DATASHEET this pins are powered by VMMC1, Vdds_mmc1 is supplying 3.0V…
Hi:
I can't suspend my omap3515.
if I have already set all powerdomain(except MPU and Core) to retention or off mode, the cpu will do a transition to retention.
But I found the peripheral powerdomain always active. How to change it to retention…
Hi Field team.
Please refer below inputs:
1. Can I share the schematics for review over E2E
We do not support schematics review request by field teams or customer over E2E. TI field team will have to submit schematics review request over email.
2. If not…