Other Parts Discussed in Thread: OMAP3503 , OMAP3515 , TFP410 We're beginning development on a video application that involves decoding a stream of JPEG images and encoding the stream into HDMI. I was given the recommendation to check out the OMAP devices…
Hi Tsvetolin,
Thanks for your reply. I noticed DM37XX were listed but the BSDLs were different so I was confused.
Should I edit BSDL file and add icepick register and instruction codes as in omap 3525 BSDL file? Or is there file where the icepick is defined…
Other Parts Discussed in Thread: DM3730 , OMAP3515 Hi ,
I have a problem with the omap3515 and dm3730 board . My boards use linux kernel 2.6.37 source code. and I use the usb ohci host function, when I initialize the mm1_txse0 pin(gpio 15) for this (original…
Other Parts Discussed in Thread: OMAP3515
I am using OMAP3515 processor (Generic CortexA8 Device) for my project and want to boot the system form UART3. The boot loader code which I am using is working fine when using emulator i.e it is able to write…
Other Parts Discussed in Thread: OMAP3515 I am using OMAP3515 processor (Generic CortexA8 Device) for my project and want to boot the system form UART3. The boot loader code which I am using is working fine when using emulator i.e it is able to write the…
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
Other Parts Discussed in Thread: OMAP3530 , OMAP3515 , OMAP3503 Hello everyone,
I just did the update of CCS V5.3 but I can't seem to find my device in the ARM component list.
I try to the run the OMAP3530 on a BeagleBoard but CCS only shows OMAP3503…
Some of the new 3517 SOCs have a different revision information - can you try below steps to fix this ? A later version of the kit should have this fixed.
- Locate the file "/usr/bin/cputype" in your filesystem
- Apply below patch (look…