Other Parts Discussed in Thread: OMAP3525 , OMAP3530 , TPS65930 To whom i am concerned,
We company is about to developing a equipment based on omap3525, and an USB3320 PHY is attached as a method to debug and upgrade. The equipment should be able to communicated…
Brian,
Thank you very much.
That indeed was the solution.
Our product uses an SD card that is not removable, so that would seem to me a perfectly safe configuration for the kernel.
Best regards,
Pete
Steve,
I am interested in doing this for 16-bit YUV422 but I am fairly new to the OMAP DSS. Could you elaborate a little on how to "basically configure the DSS to bypass all features and simply dump the frame buffer" using the omap2 driver for linux-2…
Other Parts Discussed in Thread: TUSB2551A , OMAP3525 Hi. We have a custom board which uses an omap3525 and a TUSB2551A transceiver. We have the following set up on the hardware: omap ------------ transceiver
gpio 100 ------------speed
gpio 101 -----…
Other Parts Discussed in Thread: OMAP3525 , OMAP3530 , TPS65930 Hi folks,
now that we have a new (and bigger) run of boards manufactured, an old bug popped up again:
First some history information: For a new project we're using an OMAP3525 together with…
Other Parts Discussed in Thread: TPS65950 , OMAP3525 Can anyone tell me in what sequence(flow) or what all steps we need to do for doing power managment using OMAP 3525 & TPS65950?
any detail flowchart is there for the entire core power management?
Hi,
What is the nominal voltage level for VDD1 & VDD2 supplies while enabling smart reflex? Is that the same voltage level as like when disabling the smart reflex or changes are there.
How to set the threshold voltages for the OPPs when smart reflex…
Other Parts Discussed in Thread: OMAP3525 HI - we've got a new board with an OMAP3525 and are using CCS3.3. We'd like to be able to program the nand flash - can CCS be used for this?
Thanks Mark.
From your test results, it does look like the state on this pin is "L" on reset as per the data sheet. However the states are different on my PWB with the CUS package. I'm seeing a 0V state even with a 1Kohm pull-up during reset.…