Part Number: OMAP5912 In manuals for omap5912 i find that text: JTAP controller handles standard IEEE JTAG interfaces. Boundary scan chain is implemented in OMAP5912. Where i can find bsdl file for this ic?
Other Parts Discussed in Thread: OMAP5912 if user mode found some issues have happed, we will use a software way to restart the system. the method is like this:
AMR will disable all the interrupt, then use the register to put the DSP into a reset state…
Other Parts Discussed in Thread: OMAP5912 Tool/software: Code Composer Studio Hi All,
I am using OMAP5912 board with JTAG Emulator,using a Code composer studio2,
I am trying to load a led.out file but getting a error "Data verification failed at address…
I want to use interrupt from GPIO4 module on DSP side. This module connect to Level 2 interrupt handler. I use CCS 3.3 and DSP BIOS 5.31.02. In DSP BIOS configuration only Level 1 handler interrupt, but exist HWI_INT3 vector, which use by interrupt handler…
Hi. I have the following kit: http://omap.spectrumdigital.com/osk5912/ . This board contains the OMAP 5912 DSP chip.
To develop an application in linux environment, it came with a CD which contains the installer for Montavista Linux Pro version 3.1. For…
Other Parts Discussed in Thread: OMAP5912 What documentation will provide:
1) What
is the OMAP5912 Power on Reset initialization timing....from OMAP5912 reset
input assertion to initial Local Bus Boot Flash chipselect assertion.
2) What
is the OMAP5912…