Part Number: OMAPL137-HT Hi team,
I got a question from customer.
"I am designing a board using OMAPL137BPTPH (the high temp component, 176-pin package) and I cannot find the EMU pins for the JTAG emulators. How do I perform JTAG emulation, debugging…
Part Number: OMAPL137-HT Other Parts Discussed in Thread: OMAP-L137 Hello,
The OMAPL137-HT processor is the only option for my project - active part and high temperature rated (175C).
The documentation regarding booting bare metal applications is…
Part Number: OMAPL137-HT Other Parts Discussed in Thread: OMAP-L137 I have problems with booting from flash using the Processor SDK RTOS 06_03_00_106 documentation.
I got this error using the spi_flash_writer.out from Processor SDK RTOS 06_03_00_106…
Part Number: OMAPL137-HT HI,
In our project we have shortage of SPI interfaces.
We would like to use McASP0 in place of SPI to communicate with HI-3111 which supports Serial Peripheral Interface (SPI) (20MHz).. We would like to read/write bytes…
Part Number: OMAPL137-HT Other Parts Discussed in Thread: OMAPL138 , OMAP-L138 Hi team,
I received some questions regarding the L137 Device
I have specific questions about IPC / CDC that you can hopefully get answered
Does IPC work on the OMAPL138…
Part Number: OMAPL137-HT Other Parts Discussed in Thread: OMAP-L137 , MSP430F2619S-HT , SM470R1B1M-HT , SM320F2812-HT , SM320F28335-HT Hi,
Is there any help available to start working with OMAPL137-HT and program it? I found the datasheet but for me…
Part Number: OMAPL137-HT Other Parts Discussed in Thread: MSP430FR5739
Hi,
On our board, we would be using a fpga and omapl137-ht. Is it possible to daisy-chain them together?
I saw BSDL file is available for omapl137, so I assume the answer is…
Part Number: OMAPL137-HT Other Parts Discussed in Thread: OMAPL138
Tool/software: Code Composer Studio
Hi,
This might be a quick setting or configuration issue. I have CCS7.4 installed and trying to rebuild an example --- OMAPL137_bf_rt project…
Part Number: OMAPL137-HT Hi, All
I have two types of board with OMAPL137. One of the two types, is designed without "Power-on sequence." At first both types were fully functional but, few monthes later, one without the "Power-on sequence" had a common…
Part Number: OMAPL137-HT Other Parts Discussed in Thread: OMAP-L137 , Tool/software: Code Composer Studio Hello.
In the datasheet for the OMAP-L137 figure 6-12 it clearly shows a flash connected to the processor's EMIFA using the open NAND flash interface…