Part Number: ONET4201LD Other Parts Discussed in Thread: ONET4211LD , Hello Team,
is it possible to use two ONET4201LD or ONET4211LD in parallel to get to current of about 170mA?
In the datasheet, I could not find a specification for the delay between input…
Hi Nasser,
the last comment is to the ONET1141L which should be capable of directly driving laser diode with anode from BIAS and MOD+.
The option with current mirrors was for suggested for the ONET4201LD.
Please see following schematics original (left…
Part Number: ONET4201LD Hello Team,
we are considering having two ONET4201 in parallel to increase the max current.
...not optimal from the jitter perspective that may come out, which may kill the signal.
On the other hand we have the option to calibrate…
Part Number: ONET4201LD Is there any restriction (other than validation for operation by TI) on running either of these devices slower than 155 Mbps? Is the minimum spec due to hardware limitations (e.g., internal ac coupling of clocks) or is this only…
Part Number: ONET4201LD *Can the ONET4201 turn on the LD by inputting the following pulse signal to DIN+?
*Is there an evaluation board for ONET4201?
* Laser driver_20230405.pdf Is there any other TI IC that can control the LD?
Part Number: ONET4201LD Other Parts Discussed in Thread: ONET4211LD , Hello there,
I would like to ask whether you offer in portfolio any laser diode driver capable of data rate 100Mbps?
I just found two of them: ONET4201LD, ONET4211LD starting at 155Mbps…
Part Number: ONET4201LD According to the description of ONET4201LD, Vbias can be set from 1V to 3.5V.
However, there is no introduction on how to set this voltage in the datasheet.
Would you please give an explanation on it?
Besides, can this LD driver…
Greetings,
I apologize for long delay and missing your post.
The only way to turn off the laser is to assert DISABLE pin.
Please let me know the status on this issue.
Regards ,, Nasser
Part Number: ONET4201LD Hi
I have an application where I need a transconductance amplifier/buffer with >= 400MHz of bandwidth
I can't find any off-the-shelf part for this
Are the Input buffers stages given in Figure 1 of the datasheet linear? Or…
Part Number: DP83869HM Other Parts Discussed in Thread: ONET4201LD , ONET4201PA , Hello,
I am using a DP83869HM with a ONET4201LD (for emitting) and a ONET4201PA (receiving) to send data with fiber. I have some questions :
- Should I place some termination…