Part Number: ONET4211LD Tool/software: Is it possible to obtain the reference layout for the ONET4211LD, such as was used to obtain the Single-Ended Output Voltage Electrical Eye diagrams in the ONET4211LD datasheet, Figs. 7, 8, and 9?
Part Number: ONET4211LD Hi,
Because the driver current is 400 mA in customer application, do you have any reference design to improve driver current up to 400mA?
Thanks & best regards,
Part Number: ONET4211LD Sirs,
We have an application which requires an external analog control of the modulation current in the ONET4211. We do not require any temperature compensation of the modulation current.
Normally the modulation current is programmed…
Part Number: ONET4201LD Is there any restriction (other than validation for operation by TI) on running either of these devices slower than 155 Mbps? Is the minimum spec due to hardware limitations (e.g., internal ac coupling of clocks) or is this only…
Part Number: ONET4211LD About optical output (mW) power control of ONET4211LD Please tell me in detail.
The pins related to optical output (mW) power control are recognized as follows.
(1) pin 11: MODSET
(2) pin 12: MODTC
(3) pin 21: IBMAX
(4) pin…
Part Number: ONET4211LD Collapse of floodlight waveform
Using ONET4211LD, make the laser diode emit light, Checking the floodlight waveform. * Waveform observation uses an APD module and is an oscilloscope. We are doing it at
Please let me know if there…
Part Number: ONET4211LD Dear TI team,
Would you have a Spice model of the laser driver output (i.e. differential output MOD+ and MOD-) that I could use in Spice for TI?
Thanks and best regards,
Thierry
Part Number: ONET4211LD Dear support team,
I would like to use the BIAS current source as a fixed DC current source, i.e whithout using the regulation loop. The resistor connected to the pin IBMAX should set the value of the current, according to fig…