Part Number: ONET8501V Other Parts Discussed in Thread: ONET4291VA , Hello TI!
I am in the process of replacing, in my electronics, the laser driver ONET4291VA because it is turning obsolete (LTB).
At the moment I am thinking to use ONET8501V. Can you say…
Part Number: ONET8501V Other Parts Discussed in Thread: ONET8501P Hello,
My customer is looking for an alternative solution for the DS1878.
Is there a way or device to replace DS1878 functions when using ONET8501V and/or ONET8501P?
Thank you.
JH
Part Number: ONET8501V The data sheet says [date rates from 2Gbps up to 11.3Gbps], Is it possible to use at 1Gbps? Please let me know if you have any problems or risks.
Part Number: ONET8501V If there is no load connected to the MOD+/MOD- terminals, or if a high impedance load is connected to the MOD+/MOD- terminals and the maximum output voltage level (IMod=24mA) is set, is there any problem or danger?
For example,…
Part Number: ONET8501V Hi
I'm trying to use the ONET8501V, The datasheet and the design are for 2007. I was wondering if there is another update or a new version available. would you please let me know?
Regards
Moein
Part Number: ONET8501V Other Parts Discussed in Thread: TIDA-00088 Hello,
I am reading following document.
There seems to be a projejct that runs on MSP430 for SFP+ module.
And I think it is also the firmware for TIDA-00088.
Is it available?
I would like…
Part Number: ONET8501V Hi Experts,
Our customer wants to know if the Laser Safety features are still active in open loop mode for ONET8501V, can you help to check? Thanks a lot!
Part Number: ONET8501V Hello TI team,
My communication system require a linear VCSEL driver in order to use pulse amplitude modulation (PAM) (up to 5G baud per second). For example, I would like to use PAM-4 with 5GBps to achieve 10Gbps.
Does ONET8501V…
Part Number: ONET8501V I am looking at the ONET8501V. I am looking for a reference schematic and evaluation board.
Also, there are a number of outputs on the chip that are used for monitoring (i.e. MONB, MONP, BGV). If I am not going to use these monitors…
Part Number: ONET8501V
Hi all. My customer request that ONET8501V is supplied in the state of die, not packaging because application is VCSEL driver of TOSA. So packaging product is not match for this application. Could you supply this device in state of…