Part Number: ONET1151L Other Parts Discussed in Thread: ONET1151P , , ONET8551T I am using the ONET1151L in a design. In the datasheet the modulated outputs connect to the laser via some ferrite beads however no detail is given on how to specify them. I…
Hi Shimizu,
Attached you will find a useful PDF with bonding recommendations for the ONET8501T.
ONET8551T APD Bonding (2).pdf
Best Regards,
Luis Omar Moran
High Speed Interface
SWAT Team
Hello Ivan,
The ONET8501T is a high gain TIA and there is a high chance for an oscillation to occur if a two terminal PD is used, especially with TO-can packaging. It is recommended to only use a 3 terminal GSG type PD with the ONET8501T as shown in…
Hello Eric,
Since the bandwidth of a TIA is inversely proportional to the total input capacitance (TIA input capacitance + photodiode capacitance), the large PD capacitance can reduce the BW by up to 5 times the typical value. However, it will also impact…
Ivan,
Pads 7 and 9 are internally connected on the ONET8551T. Therefore, either pad 7 or pad 9 can be used to supply the reverse bias voltage to the cathode of the PD.
Kpk,
In general, all bond wire lengths should be made as short as possible. The bond wire from the APD anode to the TIA should be in the 300um range. Also, it is highly recommended to use a header with 50ohm pins. The attached file has some recommendations…
Other Parts Discussed in Thread: ONET1151P , ONET8551T , ONET4201PA , ONET4211LD Hello,
Do we have 1G data rate optical module reference design that include schematics and layout guide ? Thank you.
BR
Patrick
Other Parts Discussed in Thread: ONET8501T , ONET8551T Dear Alex Davidson, One of my customer which is a major optic module manufacturer asked to help technical meeting with her about the ac characteristics of ONET8501T in detail. However I cannot find the…