Part Number: P82B96 Other Parts Discussed in Thread: TCA9416 , , TCA9803 , TCA9517 , TCA9509 Will I run into any issues using the P82B96 with the TCA9416 in a setup like this:
The TCA9416 is a "switch type" voltage translator, so I believe it will…
Part Number: P82B96 Other Parts Discussed in Thread: TEST2 , TCA9416 Hi TI
our produce is power shelf (PSU*6+PDB+PMC)
https://www.ti.com/solution/open-rack-server-psu
Test1:
PSU*1+PDB+PMC I2C communication is OK
Test2:
An I²C communication…
Part Number: P82B96 Other Parts Discussed in Thread: TCA9803 , Hello,
I asked about 5 days ago with the subject of "82B96: Question about using 1 peace of 82B96" and received an answer, but I received the following additional question/request.
"Would…
Part Number: P82B96 Please help answer the following two questions from a customer.
1) The customer knows the standard usage of P82B96DGKR is to use 2 between I2C communication lines in the configuration "Master -P82B96DGKR ~(cable)~ P82B96DGKR- Slave…
Part Number: P82B96 Other Parts Discussed in Thread: TCA9509 , TCA9517 Tool/software: Hello,
After taking over a project halfway through, it seems we have come unstuck by the problem everyone faces using the P82B96, the VOL specification on the S-side…
Part Number: P82B96 Other Parts Discussed in Thread: TCA9517 , HI team,
I'm using P82B96PWR in my design. I have connected two P82B96PWR over a long cable of 100cm. The schematic snippet is below.
On probing the Sx, Sy at both Master and Slave…
Part Number: P82B96
Tool/software:
We have 7Z SoM based board, from that we are planning to interface a microcontroller (probably STM32) with I2C where 7z SOM is master and STM32 is slave. One catch here is the two boards will be connected with a…
Part Number: P82B96 Other Parts Discussed in Thread: INA260 , INA228 , , TIDA-01608 , ISO7842 , ISOW7842 Tool/software: I've used this part (P82B96) as part of the TIDA-01608 reference design but replaced the current sensor with a INA228. The communications…
Part Number: P82B96 I am using the P82B96PWR device.
The connection between the master side and the slave side is made using a 10-meter cable, as shown in the diagram.
When the cable is 5 meters long, everything works perfectly. But when I add more…