Part Number: P82B96 Other Parts Discussed in Thread: TCA9406 , TXS0102 , Hi,
I would like to check on compatibility of this part (P82B96) for my application and if there are better options I should consider from TI. I would like to run about 12 to 18 inch…
Part Number: P82B96 Dear team,
1. Can P82B96's TX/RX and TY/RY connect to CANH/CANL directly?
2. For below application, P82B96's TX/RX and TY/RY only connect to one CAN transceiver which means Tx/Ty connect to 1042's Tx at the same time and Rx…
Part Number: P82B96 Hello team,
Could you please help me to interpret the D/S?
1.When Low is input to Txy/Rxy, the output low voltage should be 0.88V, which is higher than Txy buffer high threshould 0.7V. But this is ok because Txy buffer is open-collector…
Part Number: P82B96 Hi, I want to make communication between MCU and four I2C devices (accelerometer) without changing the I2C address.
In my current design I am using multiplexer in between MCU and Four P82B96 buffers and it is working fine.
i.e. MCU(Master…
Part Number: P82B96 Other Parts Discussed in Thread: TCA9617B , Hi Team,
We have a customer using P82B96DG4 in their application. She noticed some noise and slow rise of SCL and SDA signals as shown in the waveform below. The SCL and SDA pins are connected…
Part Number: P82B96 Other Parts Discussed in Thread: TIDA-060013 , TCA4311 , , TCA4311A , TCA9517
Hi,
We have implemented the suggested design that is recommended in TIDA-060013
https://www.ti.com/lit/ug/tiduei0/tiduei0.pdf?ts=1611661428995&ref_url=https…
Part Number: P82B96 Other Parts Discussed in Thread: ISO1540 , Hello,
could you please answer if Sx/Sy side of P82B96 is compatible with B -side of ISO1540? We plan to use it in multi-point application and want to be sure that will not suffer any issues…
Part Number: P82B96 Dear all,
I kindly need to know if the configuration below is allowed: 5V logic slave on the buffered line between two P82B96. Total track length between two P82B96 is about 10cm + 5cm cable with two JST 1mm pitch connectors.
Many…
Part Number: P82B96 Hi team,
I read the application note TIDA060013 which uses P82B96. Our customer wants to use such I2C communication with long differential cable, but the device is non-automotive device.
Is there AECQ100 device for I2C communication…
Hi Shlomi,
The diagram you shared looks good. All Vol - Vil combinations are compatible based for typical datasheet specifications and the placement of of pull-up resistors is correct. I will advise that there is possibility for incompatible output voltages…